T1042 FMAN Microcode Binary

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

T1042 FMAN Microcode Binary

ソリューションへジャンプ
3,176件の閲覧回数
mdursun
Contributor II

Hello,

We have a board design where we use T1042. We are trying to adapt it to our own card by changing the BSP prepared according to the T1042D4RDB reference card with the Linux - QORIQ SDK v2.0 software. Currently, we are stuck in the ethernet part. As far as I understand, we need a code snippet called FMAN microcode to be able to stand up the ethernet side in U-BOOT. But we couldn't find it among the T1042D4RDB project files.

Where are the source files of FMAN microcode in T1042D4RDB SDK project?

Is there a command other than the bitbake u-boot command to generate the FMAN microcode binary?

Best Regards,

ラベル(1)
タグ(3)
0 件の賞賛
返信
1 解決策
3,158件の閲覧回数
khushbur
NXP TechSupport
NXP TechSupport
2 返答(返信)
3,159件の閲覧回数
khushbur
NXP TechSupport
NXP TechSupport
3,149件の閲覧回数
mdursun
Contributor II

Hi @khushbur,

Thank you very much for the information. It solved my problem.

I could not understand the need for an additional binary file to activate FMAN. Why it is not included in the u-boot-sdcard-2016.09+fslgit-r0.bin file of the board?

Best Regards,

0 件の賞賛
返信