T1040 voltage ID feature

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

T1040 voltage ID feature

Jump to solution
2,709 Views
fdm
Contributor IV

Hi,

There's no mention of the voltage ID feature in the current revisions (rev.1) of the T1040 Data Sheet and Design Checklist.

But the T1040 Reference Manual says that "Boot software must read FUSESR and translate the values into the appropriate commands to set the voltage output value of an external voltage regulator."

Is that requirement of the voltage ID feature usage really mandatory for the T1040?

Regards,

Denis

Labels (1)
Tags (2)
0 Kudos
Reply
1 Solution
2,546 Views
ufedor
NXP Employee
NXP Employee

The voltage ID has been defeatured for the T1040.

The cited RM statement has to be discarded.


Best regards,
Fedor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

1 Reply
2,547 Views
ufedor
NXP Employee
NXP Employee

The voltage ID has been defeatured for the T1040.

The cited RM statement has to be discarded.


Best regards,
Fedor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------