T1040 voltage ID feature

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

T1040 voltage ID feature

ソリューションへジャンプ
2,695件の閲覧回数
fdm
Contributor IV

Hi,

There's no mention of the voltage ID feature in the current revisions (rev.1) of the T1040 Data Sheet and Design Checklist.

But the T1040 Reference Manual says that "Boot software must read FUSESR and translate the values into the appropriate commands to set the voltage output value of an external voltage regulator."

Is that requirement of the voltage ID feature usage really mandatory for the T1040?

Regards,

Denis

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 解決策
2,532件の閲覧回数
ufedor
NXP Employee
NXP Employee

The voltage ID has been defeatured for the T1040.

The cited RM statement has to be discarded.


Best regards,
Fedor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

1 返信
2,533件の閲覧回数
ufedor
NXP Employee
NXP Employee

The voltage ID has been defeatured for the T1040.

The cited RM statement has to be discarded.


Best regards,
Fedor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------