T1024 NOR Flash Connection

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

T1024 NOR Flash Connection

Jump to solution
1,762 Views
bltuna
Contributor II

Hi,

In T1024 reference manual, there is an example of x16 external latch based NOR Flash connection. It's mentioned in the example that a shift value of 5 is used in that example. However, I think the value shouldn't be 5 for both, should be 5 for x8 flash and 6 for x16 flash. If that so, the shift value should be 7 for a 25 bit x16 NOR Flash, right?

Capture1.PNG

Capture2.PNG

Labels (1)
Tags (2)
0 Kudos
Reply
1 Solution
1,606 Views
alexander_yakov
NXP Employee
NXP Employee

From the T1024 side, each address value always addresses one byte regardless of port size, so address value output to address lines is not changed depending on port size. The only least significant bit becomes not used for connection. For 8 bit mode all address lines are used, for 16 bit mode each address addresses 2 bytes, so least significant address line becomes unused. This is shown as unused A26 at the above figure. If this address line is left unconnected, than you do not need to change anything in address shifting.


Have a great day,
Alexander

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,607 Views
alexander_yakov
NXP Employee
NXP Employee

From the T1024 side, each address value always addresses one byte regardless of port size, so address value output to address lines is not changed depending on port size. The only least significant bit becomes not used for connection. For 8 bit mode all address lines are used, for 16 bit mode each address addresses 2 bytes, so least significant address line becomes unused. This is shown as unused A26 at the above figure. If this address line is left unconnected, than you do not need to change anything in address shifting.


Have a great day,
Alexander

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply