T1024 MDIO

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

T1024 MDIO

4,648件の閲覧回数
BharathiG
Contributor II

Need timing impact on wait of command completion event. The time taken to wait for setting of CMP is consistent for hardware, or it will be changing with variation of environmental factor (temperature or electromagnetic effect) or any other factors?

 

BharathiG_0-1669007555576.png

The above information will be useful to understand deterministic and consistent hardware behavior for a considered Software.

If the time is varying, is there any factor how much it varies?

0 件の賞賛
返信
5 返答(返信)

4,588件の閲覧回数
June_Lu
NXP TechSupport
NXP TechSupport

According to the reply last time, the calculation is right.

Variability is for every frame.

0 件の賞賛
返信

4,594件の閲覧回数
BharathiG
Contributor II

Thanks for your reply.

we are considering this for Worst case execution time. Attached the MDIO_Clock_cal.docx, let me know if the calculation is fine?. The variation factor is for complete frame or for each bit?

 

0 件の賞賛
返信

4,610件の閲覧回数
June_Lu
NXP TechSupport
NXP TechSupport

CMP represents the completion of the entire MDIO transaction.

 

For Clause 22, an MDIO ‘frame’ is either 32 or 64 bits, depending on whether preamble is enabled.

For Clause 45, a transaction may involve one or two frames, depending on whether an address frame is required.

 

Each bit of a frame takes 1 MDC cycle.

 

There is time before and after the frame which I would expect to be 1-2 MDC cycles long, +/- 1 MDC cycle.

The variability is due to two factors:

[1] Variable number of platform/2 cycles to next MDC edge (up to 1 MDC cycle)

[2] Variable sampling time when transferring from MDC domain to platform/2 domain (+/- 1 platform/2 clock), since they are async on receive side

 

The second could also vary with PVT. It would be at most +/- 1 MDC cycle.

0 件の賞賛
返信

4,624件の閲覧回数
BharathiG
Contributor II

Refer T1024DPAARM, Rev0 page number - 6-47

0 件の賞賛
返信

4,629件の閲覧回数
June_Lu
NXP TechSupport
NXP TechSupport

Would you share which document? It's a good idea to share page numbers.

0 件の賞賛
返信