T1024 IFC do not work

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

T1024 IFC do not work

ソリューションへジャンプ
7,962件の閲覧回数
hankjeon
Contributor II

I made a custom board using T1024, and set RCW source for 16-bit NOR Flash.

However, CS0# signal keeps HIGH during POR sequence.

From Trace32 I confirmed RCW source is set correctly.

Using Trace32, CPU registers and DDR can be accessed.

What am I missed? What do I check first ?

タグ(2)
1 解決策
7,082件の閲覧回数
hankjeon
Contributor II

I am sorry for the late reply.

My problem was with the pull-down resistor on pin D8.(IFC_A20)

After removing it, my borad worked well.

I designed a board by referring to the T1024RDB schematic.

The resistor is R13 on sheet 4.

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
7,159件の閲覧回数
Jaygao
Contributor I

I also meet this problem,how do you resolve this problem

0 件の賞賛
返信
7,083件の閲覧回数
hankjeon
Contributor II

I am sorry for the late reply.

My problem was with the pull-down resistor on pin D8.(IFC_A20)

After removing it, my borad worked well.

I designed a board by referring to the T1024RDB schematic.

The resistor is R13 on sheet 4.

0 件の賞賛
返信
7,894件の閲覧回数
Hector_Villarruel
NXP TechSupport
NXP TechSupport

Dear @hankjeon 

I highly recommend you to check the RCW file, could you share with me your RCW file?
I think the problem is in the RCW, I believe that the NOR flash is not configured correctly on the RCW,
On the RCW source section in Code Warrior, you have to select "Serial NOR", then click on the check box and then and check for errors.

Please refer to the attached image for reference.

Best Regards,

Hector Villarruel

 

0 件の賞賛
返信
7,156件の閲覧回数
Jaygao
Contributor I
is it relative to the rcw flie?the cs0 should keep low when the power on if set as the rcw source as 16bit nor flash
0 件の賞賛
返信