T1024 IFC do not work

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

T1024 IFC do not work

跳至解决方案
8,052 次查看
hankjeon
Contributor II

I made a custom board using T1024, and set RCW source for 16-bit NOR Flash.

However, CS0# signal keeps HIGH during POR sequence.

From Trace32 I confirmed RCW source is set correctly.

Using Trace32, CPU registers and DDR can be accessed.

What am I missed? What do I check first ?

标记 (2)
1 解答
7,172 次查看
hankjeon
Contributor II

I am sorry for the late reply.

My problem was with the pull-down resistor on pin D8.(IFC_A20)

After removing it, my borad worked well.

I designed a board by referring to the T1024RDB schematic.

The resistor is R13 on sheet 4.

在原帖中查看解决方案

0 项奖励
回复
4 回复数
7,249 次查看
Jaygao
Contributor I

I also meet this problem,how do you resolve this problem

0 项奖励
回复
7,173 次查看
hankjeon
Contributor II

I am sorry for the late reply.

My problem was with the pull-down resistor on pin D8.(IFC_A20)

After removing it, my borad worked well.

I designed a board by referring to the T1024RDB schematic.

The resistor is R13 on sheet 4.

0 项奖励
回复
7,984 次查看
Hector_Villarruel
NXP TechSupport
NXP TechSupport

Dear @hankjeon 

I highly recommend you to check the RCW file, could you share with me your RCW file?
I think the problem is in the RCW, I believe that the NOR flash is not configured correctly on the RCW,
On the RCW source section in Code Warrior, you have to select "Serial NOR", then click on the check box and then and check for errors.

Please refer to the attached image for reference.

Best Regards,

Hector Villarruel

 

0 项奖励
回复
7,246 次查看
Jaygao
Contributor I
is it relative to the rcw flie?the cs0 should keep low when the power on if set as the rcw source as 16bit nor flash
0 项奖励
回复