T1024 IFC connection with MRAM(SRAM)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

T1024 IFC connection with MRAM(SRAM)

ソリューションへジャンプ
3,316件の閲覧回数
safeerkt
Contributor II

Hi ,

We are planning to use QorIQ T1024 processor in one of our design.We want to interface a MRAM(SRAM archit) to the processor through IFC.We have a 4MBit MRAM with 19 address line and 8 data bit.could you please help me with the address and data mapping from processor to the MRAM part? Which all address and DA lines should I use and how should i map it?

Many Thanks,

Safeer.

ラベル(1)
1 解決策
2,964件の閲覧回数
alexander_yakov
NXP Employee
NXP Employee

Please look T1024 Reference Manual, Figure 23-65 "IFC to 8-bit NOR device interface" for example SRAM-like device connection. Please note reversal mapping - AD[0:7] to D[7:0] and AD[0:15]+ADDR[16:31] to A[31:0].


Have a great day,
Alexander

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

4 返答(返信)
2,964件の閲覧回数
safeerkt
Contributor II

Hi Alexander,

Thank you very much for your support.

Just one more clarification,

In our SRAM part we have 19 address lines.So can I follow the below address mapping?

 T1024 side                            SRAM side

-----------------                        ------------------

ADDR[16:31]                        A[15:0]

AD[12:15]                             A[19:16]

Could you please confirm this?

Many Thanks,

Safeer.

0 件の賞賛
返信
2,964件の閲覧回数
alexander_yakov
NXP Employee
NXP Employee

Yes, I do not see anything incorrect.

2,964件の閲覧回数
safeerkt
Contributor II

Thanks Mr.Alexander.

0 件の賞賛
返信
2,965件の閲覧回数
alexander_yakov
NXP Employee
NXP Employee

Please look T1024 Reference Manual, Figure 23-65 "IFC to 8-bit NOR device interface" for example SRAM-like device connection. Please note reversal mapping - AD[0:7] to D[7:0] and AD[0:15]+ADDR[16:31] to A[31:0].


Have a great day,
Alexander

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------