Hi ,
We are planning to use QorIQ T1024 processor in one of our design.We want to interface a MRAM(SRAM archit) to the processor through IFC.We have a 4MBit MRAM with 19 address line and 8 data bit.could you please help me with the address and data mapping from processor to the MRAM part? Which all address and DA lines should I use and how should i map it?
Many Thanks,
Safeer.
Solved! Go to Solution.
 alexander_yakov
		
			alexander_yakov
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Please look T1024 Reference Manual, Figure 23-65 "IFC to 8-bit NOR device interface" for example SRAM-like device connection. Please note reversal mapping - AD[0:7] to D[7:0] and AD[0:15]+ADDR[16:31] to A[31:0].
Have a great day,
Alexander
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Alexander,
Thank you very much for your support.
Just one more clarification,
In our SRAM part we have 19 address lines.So can I follow the below address mapping?
T1024 side SRAM side
----------------- ------------------
ADDR[16:31] A[15:0]
AD[12:15] A[19:16]
Could you please confirm this?
Many Thanks,
Safeer.
 alexander_yakov
		
			alexander_yakov
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Yes, I do not see anything incorrect.
Thanks Mr.Alexander.
 alexander_yakov
		
			alexander_yakov
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Please look T1024 Reference Manual, Figure 23-65 "IFC to 8-bit NOR device interface" for example SRAM-like device connection. Please note reversal mapping - AD[0:7] to D[7:0] and AD[0:15]+ADDR[16:31] to A[31:0].
Have a great day,
Alexander
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------