T1024 DDR

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
3,367件の閲覧回数
BharathiG
Contributor II

Hi,

 

During the DDR initialization software is setting D_INIT bit and after initialization is done software waits for this bit to be cleared. Hardware will clear this bit after the initialization is complete.  Clearing of D_INIT bit is consistent for all T1024 hardware’s or it will changing with variation of environmental factor (temperature or electromagnetic effect) or any other factors?

BharathiG_1-1660727558895.png

 

0 件の賞賛
返信
1 解決策
3,333件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

The clearing of D_INIT bit is done 100% of time by HW if DDR initialization completes.

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
3,303件の閲覧回数
BharathiG
Contributor II

I accept what you said and we are seeing the clearing of D_INIT bit by hardware. Powerup to powerup will their be any variations (timing variations) in clearing this bit ? Will it be consistently clearing the bit?

0 件の賞賛
返信
3,282件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

For the same board type (same HW and SW/settings), the time it takes to clear the D_INIT would be constantly the same.

0 件の賞賛
返信
3,334件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

The clearing of D_INIT bit is done 100% of time by HW if DDR initialization completes.

0 件の賞賛
返信