T1024 DDR

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

T1024 DDR

Jump to solution
3,388 Views
BharathiG
Contributor II

Hi,

 

During the DDR initialization software is setting D_INIT bit and after initialization is done software waits for this bit to be cleared. Hardware will clear this bit after the initialization is complete.  Clearing of D_INIT bit is consistent for all T1024 hardware’s or it will changing with variation of environmental factor (temperature or electromagnetic effect) or any other factors?

BharathiG_1-1660727558895.png

 

0 Kudos
Reply
1 Solution
3,354 Views
yipingwang
NXP TechSupport
NXP TechSupport

The clearing of D_INIT bit is done 100% of time by HW if DDR initialization completes.

View solution in original post

0 Kudos
Reply
3 Replies
3,324 Views
BharathiG
Contributor II

I accept what you said and we are seeing the clearing of D_INIT bit by hardware. Powerup to powerup will their be any variations (timing variations) in clearing this bit ? Will it be consistently clearing the bit?

0 Kudos
Reply
3,303 Views
yipingwang
NXP TechSupport
NXP TechSupport

For the same board type (same HW and SW/settings), the time it takes to clear the D_INIT would be constantly the same.

0 Kudos
Reply
3,355 Views
yipingwang
NXP TechSupport
NXP TechSupport

The clearing of D_INIT bit is done 100% of time by HW if DDR initialization completes.

0 Kudos
Reply