Second Thread Initailization Error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Second Thread Initailization Error

1,250件の閲覧回数
stevenstarnes
Contributor III

Hello,

   I am trying to run Core 0 thread 1 after initializing the core from thread 0 on the T2080. However after setting the thread initial machine state register to match thread 0, and the next instruction address to 0xFFFF_FFFC and then setting the thread enable bit to 1, nothing happens. I have a printf statement displaying the core number and thread number which works for core0 thread0 but nothing appears for core0 thread1. I am using the standard ROM initialization code for the ROM target.

ラベル(1)
0 件の賞賛
返信
0 返答(返信)