Second Thread Initailization Error

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Second Thread Initailization Error

1,278 次查看
stevenstarnes
Contributor III

Hello,

   I am trying to run Core 0 thread 1 after initializing the core from thread 0 on the T2080. However after setting the thread initial machine state register to match thread 0, and the next instruction address to 0xFFFF_FFFC and then setting the thread enable bit to 1, nothing happens. I have a printf statement displaying the core number and thread number which works for core0 thread0 but nothing appears for core0 thread1. I am using the standard ROM initialization code for the ROM target.

标签 (1)
0 项奖励
回复
0 回复数