NOR Flash Control Machine

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NOR Flash Control Machine

2,557 Views
oguzhanemre_ard
Contributor II

Hello,

I have several questions with regards to the IFC's NOR Flash Control Machine:

1) I am having difficulty in distinguishing the NOR FCM type between muxed or unmuxed(parallel). T1040 ref man gives timings of two different concept but how should we consider it? Does the term "muxed" mean IFC - Flash connection (where there exist a D-type latch IC in between as in T1042D4RDB_revA) or internal latch based NOR device? Which one should be considered for T1042D4RDB_revA design?

2) For Figure 24-42 in T1040 ref man under heading 24.6.5, the time interval between the assertion of OE and the assertion of Sample is not specified(as following). What is the reason for that?

Capture.PNG

3) What are the default (NOR Flash Mode) flash timing parameters (for BOOT, for instance)?

Kind regards,

Labels (1)
0 Kudos
Reply
2 Replies

2,477 Views
ufedor
NXP Employee
NXP Employee

1) Muxed corresponds to the address data multiplexed (ADM) NOR devices connection.

2) The timing is TRAD.

3) Refer to the QorIQ T1040 Reference Manual, Table 24-4. Default values of FTIMnCS0 during boot.

2,477 Views
oguzhanemre_ard
Contributor II

So, which timing is applied for reference design board T1042D4RDB_revA's NOR Flash?

0 Kudos
Reply