LCD Interface with 1042RDB

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LCD Interface with 1042RDB

1,450 Views
athershehzad
Contributor III

How to interface TFT LCD(LQ150X1LW71N) that is shown in reference schematic with T1042RDB? The brightness control connectors of the LCD panel are two pin connector and there is 3 pin connector on board(J16, J17) . Similarly there are two connectors(J16,J17) on board relevant to LCD's brightness whereas there are four connectors(CN2,3,4,5) on LCD panel.

Labels (1)
0 Kudos
Reply
2 Replies

1,274 Views
ufedor
NXP Employee
NXP Employee

It is required to use DC to AC inverter.

For example, DMD43246:

http://www.ergpower.com/pdf30/DmD43246.pdf

The RDB 16-2 provides 12V for the inverter.

To control ON/OFF and brightness it is needed to connect:

RDB      Inverter

J17-1      J1-5

J17-3      J1-6

0 Kudos
Reply

1,274 Views
athershehzad
Contributor III

Then how the brightness is controlled of the LCD.
What is will be connected to J17 ?

0 Kudos
Reply