LCD Interface with 1042RDB

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LCD Interface with 1042RDB

2,141件の閲覧回数
athershehzad
Contributor III

How to interface TFT LCD(LQ150X1LW71N) that is shown in reference schematic with T1042RDB? The brightness control connectors of the LCD panel are two pin connector and there is 3 pin connector on board(J16, J17) . Similarly there are two connectors(J16,J17) on board relevant to LCD's brightness whereas there are four connectors(CN2,3,4,5) on LCD panel.

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,965件の閲覧回数
ufedor
NXP Employee
NXP Employee

It is required to use DC to AC inverter.

For example, DMD43246:

http://www.ergpower.com/pdf30/DmD43246.pdf

The RDB 16-2 provides 12V for the inverter.

To control ON/OFF and brightness it is needed to connect:

RDB      Inverter

J17-1      J1-5

J17-3      J1-6

0 件の賞賛
返信

1,965件の閲覧回数
athershehzad
Contributor III

Then how the brightness is controlled of the LCD.
What is will be connected to J17 ?

0 件の賞賛
返信