If there is a possible to run docker or other container on yocto Linux?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

If there is a possible to run docker or other container on yocto Linux?

800 Views
eric7
Contributor I

Due to business needs, I have to isolate applications running in yocto Linux. I can think of ways to use containers, but I tried to install docker in yocto Linux without success. I am using a T4240 processor and I don’t know if there are any successful installation cases. I'd love some advice on installing the container.

0 Kudos
Reply
1 Reply

774 Views
yipingwang
NXP TechSupport
NXP TechSupport

Please download document QORIQ-SDK-2.0-IC-REV0.pdf from https://support.nxp.com/s/case/5002p00002x1B5EAAU/community-if-there-is-a-possible-to-run-docker-or-...

Then refer to the section "11.5 Docker Containers".

0 Kudos
Reply