How to enable TCL 8.6, Python 2.7.18 and SSHv2 (OpenSSH_7.6p1) in T1040RDB

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to enable TCL 8.6, Python 2.7.18 and SSHv2 (OpenSSH_7.6p1) in T1040RDB

ソリューションへジャンプ
15,681件の閲覧回数
Suraj_Prakash
Contributor II

Hi,

   I want to have the additional software features on the T1040rdb which are mentioned below:

         1. TCL 8.6
         2. Python 2.7.18
         3. SSHv2 (OpenSSH_7.6p1)

Please suggest how to enable those features.

ラベル(1)
0 件の賞賛
返信
1 解決策
15,503件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Please delete "python-subprocess" in sources/meta-openembedded/meta-oe/recipes-benchmark/libhugetlbfs/libhugetlbfs_git.bb.

Please add the following in sources/poky/meta/recipes-devtools/python/python_2.7.18.b.

RDEPENDS_remove += "python-re python-contextlib python-netclient"

Then run the following command.

$ bitbake libhugetlbfs -c cleansstate

$ bitbake python -c cleansstate

$ bitbake fsl-image-core

元の投稿で解決策を見る

0 件の賞賛
返信
28 返答(返信)
15,504件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Please delete "python-subprocess" in sources/meta-openembedded/meta-oe/recipes-benchmark/libhugetlbfs/libhugetlbfs_git.bb.

Please add the following in sources/poky/meta/recipes-devtools/python/python_2.7.18.b.

RDEPENDS_remove += "python-re python-contextlib python-netclient"

Then run the following command.

$ bitbake libhugetlbfs -c cleansstate

$ bitbake python -c cleansstate

$ bitbake fsl-image-core

0 件の賞賛
返信
2,497件の閲覧回数
sandeepk1980
Contributor I

Hi

    i have followed all the steps listed in this thread and was successful in getting python 2.7.18 on my card.

But when i try to run python command i get this error

root@t1040d4rdb:/usr/lib64/python2.7# python --version
Python 2.7.18

root@t1040d4rdb:~# python
ImportError: No module named site


root@t1040d4rdb:~# cd /usr/lib64/python2.7/

root@t1040d4rdb:/usr/lib64/python2.7# ls
config lib-dynload sitecustomize.py


root@t1040d4rdb:/usr/lib64/python2.7# python --version
Python 2.7.18

 

Actually there are no modules in /usr/lib64/python2.7/

earlier when we used pyhton 2.7.9, there used to be many modules in this folder

Please suggest solution

 

Thanks

0 件の賞賛
返信
2,487件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Python modules are integrated in folder /usr/SEDMELIBLEAF/python2.7/, you could move them to file /usr/lib64/python2.7/ folder on the target board.

0 件の賞賛
返信
2,568件の閲覧回数
Suraj_Prakash
Contributor II

Hi,

       Thankyou so much for your support

0 件の賞賛
返信
2,584件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

After adding the following line in sources/poky/meta/recipes-devtools/python/python_2.7.18.bb

RDEPENDS_remove += "python-re python-contextlib"

Please rebuild python

$bitbake python -c cleansstate

$bitbake fsl-image-core

0 件の賞賛
返信
2,583件の閲覧回数
Suraj_Prakash
Contributor II

Hi,

      still stuck with the same error

bitbake fsl-image-core
WARNING: Host distribution "Ubuntu-16.04" has not been validated with this version of the build system; you may possibly experience unexpected failures. It is recommended that you use a tested distribution.
Loading cache: 100% |#####################################################################################################################################################| ETA: 00:00:00
Loaded 6068 entries from dependency cache.
NOTE: Resolving any missing task queue dependencies
NOTE: preferred version 2.7.9 of python not available (for item python)
NOTE: versions of python available: 2.7.18
NOTE: preferred version 2.7.9 of python not available (for item python-subprocess)
NOTE: versions of python available: 2.7.18
NOTE: preferred version 2.7.9 of python not available (for item python-datetime)
NOTE: versions of python available: 2.7.18
NOTE: preferred version 2.7.9 of python not available (for item python-json)
NOTE: versions of python available: 2.7.18
NOTE: preferred version 2.7.9 of python not available (for item python-2to3)
NOTE: versions of python available: 2.7.18
NOTE: preferred version 2.7.9 of python not available (for item python-argparse)
NOTE: versions of python available: 2.7.18
NOTE: preferred version 2.7.9 of python not available (for item python-audio)
NOTE: versions of python available: 2.7.18
NOTE: preferred version 2.7.9 of python not available (for item python-bsddb)
NOTE: versions of python available: 2.7.18
NOTE: preferred version 2.7.9 of python not available (for item python-codecs)
NOTE: versions of python available: 2.7.18
NOTE: preferred version 2.7.9 of python not available (for item python-compile)
NOTE: versions of python available: 2.7.18
NOTE: preferred version 2.7.9 of python not available (for item python-compiler)
NOTE: versions of python available: 2.7.18
NOTE: preferred version 2.7.9 of python not available (for item python-compression)
NOTE: versions of python available: 2.7.18
NOTE: preferred version 2.7.9 of python not available (for item python-contextlib)
NOTE: versions of python available: 2.7.18
NOTE: preferred version 2.7.9 of python not available (for item python-core)
NOTE: versions of python available: 2.7.18
NOTE: preferred version 2.7.9 of python not available (for item python-crypt)
NOTE: versions of python available: 2.7.18
NOTE: preferred version 2.7.9 of python not available (for item python-ctypes)
NOTE: versions of python available: 2.7.18
NOTE: preferred version 2.7.9 of python not available (for item python-curses)
NOTE: versions of python available: 2.7.18
NOTE: preferred version 2.7.9 of python not available (for item python-db)
NOTE: versions of python available: 2.7.18
NOTE: preferred version 2.7.9 of python not available (for item python-debugger)
NOTE: versions of python available: 2.7.18
NOTE: preferred version 2.7.9 of python not available (for item python-difflib)
NOTE: versions of python available: 2.7.18
NOTE: preferred version 2.7.9 of python not available (for item python-distutils)
NOTE: versions of python available: 2.7.18
NOTE: preferred version 2.7.9 of python not available (for item python-doctest)
NOTE: versions of python available: 2.7.18
NOTE: preferred version 2.7.9 of python not available (for item python-elementtree)
NOTE: versions of python available: 2.7.18
NOTE: preferred version 2.7.9 of python not available (for item python-email)
NOTE: versions of python available: 2.7.18
NOTE: preferred version 2.7.9 of python not available (for item python-fcntl)
NOTE: versions of python available: 2.7.18
NOTE: preferred version 2.7.9 of python not available (for item python-gdbm)
NOTE: versions of python available: 2.7.18
NOTE: preferred version 2.7.9 of python not available (for item python-hotshot)
NOTE: versions of python available: 2.7.18
NOTE: preferred version 2.7.9 of python not available (for item python-html)
NOTE: versions of python available: 2.7.18
NOTE: preferred version 2.7.9 of python not available (for item python-idle)
NOTE: versions of python available: 2.7.18
NOTE: preferred version 2.7.9 of python not available (for item python-image)
NOTE: versions of python available: 2.7.18
NOTE: preferred version 2.7.9 of python not available (for item python-importlib)
NOTE: versions of python available: 2.7.18
NOTE: preferred version 2.7.9 of python not available (for item python-io)
NOTE: versions of python available: 2.7.18
NOTE: preferred version 2.7.9 of python not available (for item python-lang)
NOTE: versions of python available: 2.7.18
NOTE: preferred version 2.7.9 of python not available (for item python-logging)
NOTE: versions of python available: 2.7.18
NOTE: preferred version 2.7.9 of python not available (for item python-mailbox)
NOTE: versions of python available: 2.7.18
NOTE: preferred version 2.7.9 of python not available (for item python-math)
NOTE: versions of python available: 2.7.18
NOTE: preferred version 2.7.9 of python not available (for item python-mime)
NOTE: versions of python available: 2.7.18
NOTE: preferred version 2.7.9 of python not available (for item python-mmap)
NOTE: versions of python available: 2.7.18
NOTE: preferred version 2.7.9 of python not available (for item python-multiprocessing)
NOTE: versions of python available: 2.7.18
NOTE: preferred version 2.7.9 of python not available (for item python-netclient)
NOTE: versions of python available: 2.7.18
NOTE: preferred version 2.7.9 of python not available (for item python-netserver)
NOTE: versions of python available: 2.7.18
NOTE: preferred version 2.7.9 of python not available (for item python-numbers)
NOTE: versions of python available: 2.7.18
NOTE: preferred version 2.7.9 of python not available (for item python-pickle)
NOTE: versions of python available: 2.7.18
NOTE: preferred version 2.7.9 of python not available (for item python-pkgutil)
NOTE: versions of python available: 2.7.18
NOTE: preferred version 2.7.9 of python not available (for item python-pprint)
NOTE: versions of python available: 2.7.18
NOTE: preferred version 2.7.9 of python not available (for item python-profile)
NOTE: versions of python available: 2.7.18
NOTE: preferred version 2.7.9 of python not available (for item python-pydoc)
NOTE: versions of python available: 2.7.18
NOTE: preferred version 2.7.9 of python not available (for item python-re)
NOTE: versions of python available: 2.7.18
NOTE: preferred version 2.7.9 of python not available (for item python-readline)
NOTE: versions of python available: 2.7.18
NOTE: preferred version 2.7.9 of python not available (for item python-resource)
NOTE: versions of python available: 2.7.18
NOTE: preferred version 2.7.9 of python not available (for item python-robotparser)
NOTE: versions of python available: 2.7.18
NOTE: preferred version 2.7.9 of python not available (for item python-shell)
NOTE: versions of python available: 2.7.18
NOTE: preferred version 2.7.9 of python not available (for item python-smtpd)
NOTE: versions of python available: 2.7.18
NOTE: preferred version 2.7.9 of python not available (for item python-sqlite3)
NOTE: versions of python available: 2.7.18
NOTE: preferred version 2.7.9 of python not available (for item python-sqlite3-tests)
NOTE: versions of python available: 2.7.18
NOTE: preferred version 2.7.9 of python not available (for item python-stringold)
NOTE: versions of python available: 2.7.18
NOTE: preferred version 2.7.9 of python not available (for item python-syslog)
NOTE: versions of python available: 2.7.18
NOTE: preferred version 2.7.9 of python not available (for item python-terminal)
NOTE: versions of python available: 2.7.18
NOTE: preferred version 2.7.9 of python not available (for item python-tests)
NOTE: versions of python available: 2.7.18
NOTE: preferred version 2.7.9 of python not available (for item python-textutils)
NOTE: versions of python available: 2.7.18
NOTE: preferred version 2.7.9 of python not available (for item python-threading)
NOTE: versions of python available: 2.7.18
NOTE: preferred version 2.7.9 of python not available (for item python-tkinter)
NOTE: versions of python available: 2.7.18
NOTE: preferred version 2.7.9 of python not available (for item python-unittest)
NOTE: versions of python available: 2.7.18
NOTE: preferred version 2.7.9 of python not available (for item python-unixadmin)
NOTE: versions of python available: 2.7.18
NOTE: preferred version 2.7.9 of python not available (for item python-xml)
NOTE: versions of python available: 2.7.18
NOTE: preferred version 2.7.9 of python not available (for item python-xmlrpc)
NOTE: versions of python available: 2.7.18
NOTE: preferred version 2.7.9 of python not available (for item python-zlib)
NOTE: versions of python available: 2.7.18
NOTE: preferred version 2.7.9 of python not available (for item python-misc)
NOTE: versions of python available: 2.7.18
NOTE: preferred version 2.7.9 of python not available (for item python)
NOTE: versions of python available: 2.7.18
NOTE: preferred version 2.7.9 of lib32-python not available (for item lib32-python-pickle)
NOTE: versions of lib32-python available: 2.7.18
NOTE: preferred version 2.7.9 of lib32-python not available (for item lib32-python-crypt)
NOTE: versions of lib32-python available: 2.7.18
NOTE: preferred version 2.7.9 of lib32-python not available (for item lib32-python-shell)
NOTE: versions of lib32-python available: 2.7.18
NOTE: preferred version 2.7.9 of lib32-python not available (for item lib32-python-fcntl)
NOTE: versions of lib32-python available: 2.7.18
NOTE: preferred version 2.7.9 of lib32-python not available (for item lib32-python-stringold)
NOTE: versions of lib32-python available: 2.7.18
NOTE: preferred version 2.7.9 of lib32-python not available (for item lib32-python-logging)
NOTE: versions of lib32-python available: 2.7.18
NOTE: preferred version 2.7.9 of lib32-python not available (for item lib32-python-subprocess)
NOTE: versions of lib32-python available: 2.7.18
NOTE: preferred version 2.7.9 of lib32-python not available (for item lib32-python-math)
NOTE: versions of lib32-python available: 2.7.18
NOTE: preferred version 2.7.9 of lib32-python not available (for item lib32-python-compression)
NOTE: versions of lib32-python available: 2.7.18
NOTE: preferred version 2.7.9 of lib32-python not available (for item lib32-python)
NOTE: versions of lib32-python available: 2.7.18
NOTE: preferred version 2.7.9 of lib32-python not available (for item lib32-python-textutils)
NOTE: versions of lib32-python available: 2.7.18
NOTE: preferred version 2.7.9 of lib32-python not available (for item lib32-python-io)
NOTE: versions of lib32-python available: 2.7.18
NOTE: preferred version 2.7.9 of lib32-python not available (for item lib32-python-re)
NOTE: versions of lib32-python available: 2.7.18
NOTE: preferred version 2.7.9 of lib32-python not available (for item lib32-python-lang)
NOTE: versions of lib32-python available: 2.7.18
NOTE: preferred version 2.7.9 of lib32-python not available (for item lib32-python-core)
NOTE: versions of lib32-python available: 2.7.18
NOTE: preferred version 2.7.9 of lib32-python not available (for item lib32-python-pprint)
NOTE: versions of lib32-python available: 2.7.18
NOTE: preferred version 2.7.9 of lib32-python not available (for item lib32-python-netclient)
NOTE: versions of lib32-python available: 2.7.18
NOTE: preferred version 2.7.9 of lib32-python not available (for item lib32-python-audio)
NOTE: versions of lib32-python available: 2.7.18
NOTE: preferred version 2.7.9 of lib32-python not available (for item lib32-python-image)
NOTE: versions of lib32-python available: 2.7.18
NOTE: preferred version 2.7.9 of lib32-python not available (for item lib32-python-mime)
NOTE: versions of lib32-python available: 2.7.18
NOTE: preferred version 2.7.9 of lib32-python not available (for item lib32-python-zlib)
NOTE: versions of lib32-python available: 2.7.18
NOTE: preferred version 2.7.9 of lib32-python not available (for item lib32-python-datetime)
NOTE: versions of lib32-python available: 2.7.18
NOTE: preferred version 2.7.9 of lib32-python not available (for item lib32-python-threading)
NOTE: versions of lib32-python available: 2.7.18
NOTE: preferred version 2.7.9 of lib32-python not available (for item lib32-python-sqlite3)
NOTE: versions of lib32-python available: 2.7.18
NOTE: preferred version 2.7.9 of lib32-python not available (for item lib32-python-tkinter)
NOTE: versions of lib32-python available: 2.7.18
NOTE: preferred version 2.7.9 of lib32-python not available (for item lib32-python-codecs)
NOTE: versions of lib32-python available: 2.7.18
NOTE: preferred version 2.7.9 of lib32-python not available (for item lib32-python-distutils)
NOTE: versions of lib32-python available: 2.7.18
NOTE: preferred version 2.7.9 of lib32-python not available (for item lib32-python-difflib)
NOTE: versions of lib32-python available: 2.7.18
NOTE: preferred version 2.7.9 of lib32-python not available (for item lib32-python-contextlib)
NOTE: versions of lib32-python available: 2.7.18
NOTE: preferred version 2.7.9 of lib32-python not available (for item lib32-python-xml)
NOTE: versions of lib32-python available: 2.7.18
NOTE: preferred version 2.7.9 of lib32-python not available (for item lib32-python-netserver)
NOTE: versions of lib32-python available: 2.7.18
NOTE: preferred version 2.7.9 of lib32-python not available (for item lib32-python-ctypes)
NOTE: versions of lib32-python available: 2.7.18
NOTE: preferred version 2.7.9 of lib32-python not available (for item lib32-python-mmap)
NOTE: versions of lib32-python available: 2.7.18
NOTE: preferred version 2.7.9 of lib32-python not available (for item lib32-python-debugger)
NOTE: versions of lib32-python available: 2.7.18
NOTE: preferred version 2.7.9 of lib32-python not available (for item lib32-python-unittest)
NOTE: versions of lib32-python available: 2.7.18
NOTE: preferred version 2.7.9 of lib32-python not available (for item lib32-python-email)
NOTE: versions of lib32-python available: 2.7.18
NOTE: preferred version 2.7.9 of lib32-python not available (for item lib32-python-pkgutil)
NOTE: versions of lib32-python available: 2.7.18
NOTE: preferred version 2.7.9 of lib32-python not available (for item lib32-python-bsddb)
NOTE: versions of lib32-python available: 2.7.18
NOTE: preferred version 2.7.9 of lib32-python not available (for item lib32-python-sqlite3-tests)
NOTE: versions of lib32-python available: 2.7.18
NOTE: preferred version 2.7.9 of lib32-python not available (for item lib32-python-db)
NOTE: versions of lib32-python available: 2.7.18
NOTE: preferred version 2.7.9 of lib32-python not available (for item lib32-python-doctest)
NOTE: versions of lib32-python available: 2.7.18
NOTE: preferred version 2.7.9 of lib32-python not available (for item lib32-python-curses)
NOTE: versions of lib32-python available: 2.7.18
NOTE: preferred version 2.7.9 of lib32-python not available (for item lib32-python-idle)
NOTE: versions of lib32-python available: 2.7.18
NOTE: preferred version 2.7.9 of lib32-python not available (for item lib32-python-misc)
NOTE: versions of lib32-python available: 2.7.18
NOTE: preferred version 2.7.9 of lib32-python not available (for item lib32-python-hotshot)
NOTE: versions of lib32-python available: 2.7.18
NOTE: preferred version 2.7.9 of lib32-python not available (for item lib32-python-json)
NOTE: versions of lib32-python available: 2.7.18
NOTE: preferred version 2.7.9 of lib32-python not available (for item lib32-python-profile)
NOTE: versions of lib32-python available: 2.7.18
NOTE: preferred version 2.7.9 of lib32-python not available (for item lib32-python-pydoc)
NOTE: versions of lib32-python available: 2.7.18
NOTE: preferred version 2.7.9 of lib32-python not available (for item lib32-python-mailbox)
NOTE: versions of lib32-python available: 2.7.18
NOTE: preferred version 2.7.9 of lib32-python not available (for item lib32-python-elementtree)
NOTE: versions of lib32-python available: 2.7.18
NOTE: preferred version 2.7.9 of lib32-python not available (for item lib32-python-gdbm)
NOTE: versions of lib32-python available: 2.7.18
NOTE: preferred version 2.7.9 of lib32-python not available (for item lib32-python-resource)
NOTE: versions of lib32-python available: 2.7.18
NOTE: preferred version 2.7.9 of lib32-python not available (for item lib32-python-compiler)
NOTE: versions of lib32-python available: 2.7.18
NOTE: preferred version 2.7.9 of lib32-python not available (for item lib32-python-xmlrpc)
NOTE: versions of lib32-python available: 2.7.18
NOTE: preferred version 2.7.9 of lib32-python not available (for item lib32-python-html)
NOTE: versions of lib32-python available: 2.7.18
NOTE: preferred version 2.7.9 of lib32-python not available (for item lib32-python-2to3)
NOTE: versions of lib32-python available: 2.7.18
NOTE: preferred version 2.7.9 of lib32-python not available (for item lib32-python-syslog)
NOTE: versions of lib32-python available: 2.7.18
NOTE: preferred version 2.7.9 of lib32-python not available (for item lib32-python-compile)
NOTE: versions of lib32-python available: 2.7.18
NOTE: preferred version 2.7.9 of lib32-python not available (for item lib32-python-tests)
NOTE: versions of lib32-python available: 2.7.18
NOTE: preferred version 2.7.9 of lib32-python not available (for item lib32-python-unixadmin)
NOTE: versions of lib32-python available: 2.7.18
NOTE: preferred version 2.7.9 of lib32-python not available (for item lib32-python-smtpd)
NOTE: versions of lib32-python available: 2.7.18
NOTE: preferred version 2.7.9 of lib32-python not available (for item lib32-python-terminal)
NOTE: versions of lib32-python available: 2.7.18
NOTE: preferred version 2.7.9 of lib32-python not available (for item lib32-python-readline)
NOTE: versions of lib32-python available: 2.7.18
NOTE: preferred version 2.7.9 of lib32-python not available (for item lib32-python-importlib)
NOTE: versions of lib32-python available: 2.7.18
NOTE: preferred version 2.7.9 of lib32-python not available (for item lib32-python-argparse)
NOTE: versions of lib32-python available: 2.7.18
NOTE: preferred version 2.7.9 of lib32-python not available (for item lib32-python-robotparser)
NOTE: versions of lib32-python available: 2.7.18
NOTE: preferred version 2.7.9 of lib32-python not available (for item lib32-python-multiprocessing)
NOTE: versions of lib32-python available: 2.7.18
NOTE: preferred version 2.7.9 of lib32-python not available (for item lib32-python-numbers)
NOTE: versions of lib32-python available: 2.7.18

Build Configuration:
BB_VERSION = "1.28.0"
BUILD_SYS = "x86_64-linux"
NATIVELSBSTRING = "Ubuntu-16.04"
TARGET_SYS = "powerpc64-fsl-linux"
MACHINE = "t1040d4rdb-64b"
DISTRO = "fsl-qoriq"
DISTRO_VERSION = "2.0"
TUNE_FEATURES = "m64 fpu-hard e5500"
TARGET_FPU = "hard"
meta
meta-yocto
meta-yocto-bsp = "HEAD:9a211a4a2c1bfcb292dc97d8dcac149bca9e3f1b"
meta-oe
meta-multimedia
meta-gnome
meta-networking
meta-perl
meta-python
meta-ruby
meta-filesystems
meta-webserver
meta-xfce = "HEAD:dc5634968b270dde250690609f0015f881db81f2"
meta-freescale = "HEAD:7facbdb726e2dda0515e084c2066a4b8dd99c6d2"
meta-freescale-internal = "HEAD:4829293f807e35a1111e79763294fc8b98b97810"
meta-freescale-extra = "HEAD:bee911b027e0480b034674d0ddee3fcb06d2e985"
meta-virtualization = "HEAD:042425c1d98bdd7e44a62789bd03b375045266f5"
meta-java = "HEAD:8b776ac68f9af4596be3824152bcf0bc6b67fa1d"
meta-openstack
meta-openstack-aio-deploy
meta-openstack-compute-deploy
meta-openstack-compute-test-config
meta-openstack-controller-deploy
meta-openstack-controller-test-config
meta-openstack-qemu
meta-openstack-swift-deploy
meta-cloud-services = "HEAD:d8bc0d92d0f741e2ea1e6d3d9bc6b7a091d03cfb"
meta-security = "HEAD:f9367e71f923fc7d2fb600208e2b97535ea41777"
meta-nxp-npi-1701 = "jethro-sdk-v2.0-ga-1701:11975eebce9096a3567d00ba2067a2dbd2ed4d5c"

NOTE: Preparing RunQueue
WARNING: /home/suchita/GCR/v2/QorIQ-SDK-V2.0-20160527-yocto/sources/meta-freescale/recipes-kernel/linux/linux-qoriq_4.1.bb.do_compile is tainted from a forced run
NOTE: Checking sstate mirror object availability (for 12 objects)
NOTE: Executing SetScene Tasks
NOTE: Executing RunQueue Tasks
ERROR: Unable to install packages. Command '/home/suchita/GCR/v2/QorIQ-SDK-V2.0-20160527-yocto/build_t1040d4rdb-64b/tmp/sysroots/x86_64-linux/usr/bin/smart --log-level=warning --data-dir=/home/suchita/GCR/v2/QorIQ-SDK-V2.0-20160527-yocto/build_t1040d4rdb-64b/tmp/work/t1040d4rdb_64b-fsl-linux/fsl-image-core/1.0-r0/rootfs/var/lib/smart install -y lsb@ppc64e5500 net-snmp@ppc64e5500 packagegroup-fsl-mfgtools@all python-core-2.7.18-r1@ppc64e5500 openssh@ppc64e5500 packagegroup-core-ssh-openssh@all tcl@ppc64e5500 udev-extraconf@ppc64e5500 packagegroup-core-boot@t1040d4rdb_64b packagegroup-fsl-benchmark-core@all sqlite3@ppc64e5500 run-postinsts@all udev-rules-qoriq@ppc64e5500 packagegroup-fsl-networking-core@all packagegroup-fsl-tools-core@all libpam@ppc64e5500' returned 1:
Loading cache...
Updating cache... ######################################## [100%]

Computing transaction...error: Can't install packagegroup-fsl-tools-core-1.0-r0@all: no package provides python-subprocess


ERROR: Function failed: do_rootfs
ERROR: Logfile of failure stored in: /home/suchita/GCR/v2/QorIQ-SDK-V2.0-20160527-yocto/build_t1040d4rdb-64b/tmp/work/t1040d4rdb_64b-fsl-linux/fsl-image-core/1.0-r0/temp/log.do_rootfs.27719
ERROR: Task 7 (/home/suchita/GCR/v2/QorIQ-SDK-V2.0-20160527-yocto/sources/meta-freescale/recipes-fsl/images/fsl-image-core.bb, do_rootfs) failed with exit code '1'
NOTE: Tasks Summary: Attempted 3349 tasks of which 3323 didn't need to be rerun and 1 failed.
No currently running tasks (3349 of 3350)

Summary: 1 task failed:
/home/suchita/GCR/v2/QorIQ-SDK-V2.0-20160527-yocto/sources/meta-freescale/recipes-fsl/images/fsl-image-core.bb, do_rootfs
Summary: There were 2 WARNING messages shown.
Summary: There were 2 ERROR messages shown, returning a non-zero exit code.

0 件の賞賛
返信
2,581件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Please delete "python-subprocess" in sources/meta-freescale/recipes-fsl/packagegroups/packagegroup-fsl-tools-core.bb.

0 件の賞賛
返信
2,578件の閲覧回数
Suraj_Prakash
Contributor II

Hi,

      After following the suggested solution i am getting the below errors

bitbake fsl-image-core
WARNING: Host distribution "Ubuntu-16.04" has not been validated with this version of the build system; you may possibly experience unexpected failures. It is recommended that you use a tested distribution.
Loading cache: 100% |#####################################################################################################################################################| ETA: 00:00:00
Loaded 6068 entries from dependency cache.
NOTE: Resolving any missing task queue dependencies
NOTE: preferred version 2.7.9 of python not available (for item python)
NOTE: versions of python available: 2.7.18
NOTE: preferred version 2.7.9 of python not available (for item python-datetime)
NOTE: versions of python available: 2.7.18
NOTE: preferred version 2.7.9 of python not available (for item python-json)
NOTE: versions of python available: 2.7.18
NOTE: preferred version 2.7.9 of python not available (for item python-2to3)
NOTE: versions of python available: 2.7.18
NOTE: preferred version 2.7.9 of python not available (for item python-argparse)
NOTE: versions of python available: 2.7.18
NOTE: preferred version 2.7.9 of python not available (for item python-audio)
NOTE: versions of python available: 2.7.18
NOTE: preferred version 2.7.9 of python not available (for item python-bsddb)
NOTE: versions of python available: 2.7.18
NOTE: preferred version 2.7.9 of python not available (for item python-codecs)
NOTE: versions of python available: 2.7.18
NOTE: preferred version 2.7.9 of python not available (for item python-compile)
NOTE: versions of python available: 2.7.18
NOTE: preferred version 2.7.9 of python not available (for item python-compiler)
NOTE: versions of python available: 2.7.18
NOTE: preferred version 2.7.9 of python not available (for item python-compression)
NOTE: versions of python available: 2.7.18
NOTE: preferred version 2.7.9 of python not available (for item python-contextlib)
NOTE: versions of python available: 2.7.18
NOTE: preferred version 2.7.9 of python not available (for item python-core)
NOTE: versions of python available: 2.7.18
NOTE: preferred version 2.7.9 of python not available (for item python-crypt)
NOTE: versions of python available: 2.7.18
NOTE: preferred version 2.7.9 of python not available (for item python-ctypes)
NOTE: versions of python available: 2.7.18
NOTE: preferred version 2.7.9 of python not available (for item python-curses)
NOTE: versions of python available: 2.7.18
NOTE: preferred version 2.7.9 of python not available (for item python-db)
NOTE: versions of python available: 2.7.18
NOTE: preferred version 2.7.9 of python not available (for item python-debugger)
NOTE: versions of python available: 2.7.18
NOTE: preferred version 2.7.9 of python not available (for item python-difflib)
NOTE: versions of python available: 2.7.18
NOTE: preferred version 2.7.9 of python not available (for item python-distutils)
NOTE: versions of python available: 2.7.18
NOTE: preferred version 2.7.9 of python not available (for item python-doctest)
NOTE: versions of python available: 2.7.18
NOTE: preferred version 2.7.9 of python not available (for item python-elementtree)
NOTE: versions of python available: 2.7.18
NOTE: preferred version 2.7.9 of python not available (for item python-email)
NOTE: versions of python available: 2.7.18
NOTE: preferred version 2.7.9 of python not available (for item python-fcntl)
NOTE: versions of python available: 2.7.18
NOTE: preferred version 2.7.9 of python not available (for item python-gdbm)
NOTE: versions of python available: 2.7.18
NOTE: preferred version 2.7.9 of python not available (for item python-hotshot)
NOTE: versions of python available: 2.7.18
NOTE: preferred version 2.7.9 of python not available (for item python-html)
NOTE: versions of python available: 2.7.18
NOTE: preferred version 2.7.9 of python not available (for item python-idle)
NOTE: versions of python available: 2.7.18
NOTE: preferred version 2.7.9 of python not available (for item python-image)
NOTE: versions of python available: 2.7.18
NOTE: preferred version 2.7.9 of python not available (for item python-importlib)
NOTE: versions of python available: 2.7.18
NOTE: preferred version 2.7.9 of python not available (for item python-io)
NOTE: versions of python available: 2.7.18
NOTE: preferred version 2.7.9 of python not available (for item python-lang)
NOTE: versions of python available: 2.7.18
NOTE: preferred version 2.7.9 of python not available (for item python-logging)
NOTE: versions of python available: 2.7.18
NOTE: preferred version 2.7.9 of python not available (for item python-mailbox)
NOTE: versions of python available: 2.7.18
NOTE: preferred version 2.7.9 of python not available (for item python-math)
NOTE: versions of python available: 2.7.18
NOTE: preferred version 2.7.9 of python not available (for item python-mime)
NOTE: versions of python available: 2.7.18
NOTE: preferred version 2.7.9 of python not available (for item python-mmap)
NOTE: versions of python available: 2.7.18
NOTE: preferred version 2.7.9 of python not available (for item python-multiprocessing)
NOTE: versions of python available: 2.7.18
NOTE: preferred version 2.7.9 of python not available (for item python-netclient)
NOTE: versions of python available: 2.7.18
NOTE: preferred version 2.7.9 of python not available (for item python-netserver)
NOTE: versions of python available: 2.7.18
NOTE: preferred version 2.7.9 of python not available (for item python-numbers)
NOTE: versions of python available: 2.7.18
NOTE: preferred version 2.7.9 of python not available (for item python-pickle)
NOTE: versions of python available: 2.7.18
NOTE: preferred version 2.7.9 of python not available (for item python-pkgutil)
NOTE: versions of python available: 2.7.18
NOTE: preferred version 2.7.9 of python not available (for item python-pprint)
NOTE: versions of python available: 2.7.18
NOTE: preferred version 2.7.9 of python not available (for item python-profile)
NOTE: versions of python available: 2.7.18
NOTE: preferred version 2.7.9 of python not available (for item python-pydoc)
NOTE: versions of python available: 2.7.18
NOTE: preferred version 2.7.9 of python not available (for item python-re)
NOTE: versions of python available: 2.7.18
NOTE: preferred version 2.7.9 of python not available (for item python-readline)
NOTE: versions of python available: 2.7.18
NOTE: preferred version 2.7.9 of python not available (for item python-resource)
NOTE: versions of python available: 2.7.18
NOTE: preferred version 2.7.9 of python not available (for item python-robotparser)
NOTE: versions of python available: 2.7.18
NOTE: preferred version 2.7.9 of python not available (for item python-shell)
NOTE: versions of python available: 2.7.18
NOTE: preferred version 2.7.9 of python not available (for item python-smtpd)
NOTE: versions of python available: 2.7.18
NOTE: preferred version 2.7.9 of python not available (for item python-sqlite3)
NOTE: versions of python available: 2.7.18
NOTE: preferred version 2.7.9 of python not available (for item python-sqlite3-tests)
NOTE: versions of python available: 2.7.18
NOTE: preferred version 2.7.9 of python not available (for item python-stringold)
NOTE: versions of python available: 2.7.18
NOTE: preferred version 2.7.9 of python not available (for item python-subprocess)
NOTE: versions of python available: 2.7.18
NOTE: preferred version 2.7.9 of python not available (for item python-syslog)
NOTE: versions of python available: 2.7.18
NOTE: preferred version 2.7.9 of python not available (for item python-terminal)
NOTE: versions of python available: 2.7.18
NOTE: preferred version 2.7.9 of python not available (for item python-tests)
NOTE: versions of python available: 2.7.18
NOTE: preferred version 2.7.9 of python not available (for item python-textutils)
NOTE: versions of python available: 2.7.18
NOTE: preferred version 2.7.9 of python not available (for item python-threading)
NOTE: versions of python available: 2.7.18
NOTE: preferred version 2.7.9 of python not available (for item python-tkinter)
NOTE: versions of python available: 2.7.18
NOTE: preferred version 2.7.9 of python not available (for item python-unittest)
NOTE: versions of python available: 2.7.18
NOTE: preferred version 2.7.9 of python not available (for item python-unixadmin)
NOTE: versions of python available: 2.7.18
NOTE: preferred version 2.7.9 of python not available (for item python-xml)
NOTE: versions of python available: 2.7.18
NOTE: preferred version 2.7.9 of python not available (for item python-xmlrpc)
NOTE: versions of python available: 2.7.18
NOTE: preferred version 2.7.9 of python not available (for item python-zlib)
NOTE: versions of python available: 2.7.18
NOTE: preferred version 2.7.9 of python not available (for item python-misc)
NOTE: versions of python available: 2.7.18
NOTE: preferred version 2.7.9 of python not available (for item python)
NOTE: versions of python available: 2.7.18
NOTE: preferred version 2.7.9 of lib32-python not available (for item lib32-python-pickle)
NOTE: versions of lib32-python available: 2.7.18
NOTE: preferred version 2.7.9 of lib32-python not available (for item lib32-python-crypt)
NOTE: versions of lib32-python available: 2.7.18
NOTE: preferred version 2.7.9 of lib32-python not available (for item lib32-python-shell)
NOTE: versions of lib32-python available: 2.7.18
NOTE: preferred version 2.7.9 of lib32-python not available (for item lib32-python-fcntl)
NOTE: versions of lib32-python available: 2.7.18
NOTE: preferred version 2.7.9 of lib32-python not available (for item lib32-python-stringold)
NOTE: versions of lib32-python available: 2.7.18
NOTE: preferred version 2.7.9 of lib32-python not available (for item lib32-python-logging)
NOTE: versions of lib32-python available: 2.7.18
NOTE: preferred version 2.7.9 of lib32-python not available (for item lib32-python-subprocess)
NOTE: versions of lib32-python available: 2.7.18
NOTE: preferred version 2.7.9 of lib32-python not available (for item lib32-python-math)
NOTE: versions of lib32-python available: 2.7.18
NOTE: preferred version 2.7.9 of lib32-python not available (for item lib32-python-compression)
NOTE: versions of lib32-python available: 2.7.18
NOTE: preferred version 2.7.9 of lib32-python not available (for item lib32-python)
NOTE: versions of lib32-python available: 2.7.18
NOTE: preferred version 2.7.9 of lib32-python not available (for item lib32-python-textutils)
NOTE: versions of lib32-python available: 2.7.18
NOTE: preferred version 2.7.9 of lib32-python not available (for item lib32-python-io)
NOTE: versions of lib32-python available: 2.7.18
NOTE: preferred version 2.7.9 of lib32-python not available (for item lib32-python-re)
NOTE: versions of lib32-python available: 2.7.18
NOTE: preferred version 2.7.9 of lib32-python not available (for item lib32-python-lang)
NOTE: versions of lib32-python available: 2.7.18
NOTE: preferred version 2.7.9 of lib32-python not available (for item lib32-python-core)
NOTE: versions of lib32-python available: 2.7.18
NOTE: preferred version 2.7.9 of lib32-python not available (for item lib32-python-pprint)
NOTE: versions of lib32-python available: 2.7.18
NOTE: preferred version 2.7.9 of lib32-python not available (for item lib32-python-netclient)
NOTE: versions of lib32-python available: 2.7.18
NOTE: preferred version 2.7.9 of lib32-python not available (for item lib32-python-audio)
NOTE: versions of lib32-python available: 2.7.18
NOTE: preferred version 2.7.9 of lib32-python not available (for item lib32-python-image)
NOTE: versions of lib32-python available: 2.7.18
NOTE: preferred version 2.7.9 of lib32-python not available (for item lib32-python-mime)
NOTE: versions of lib32-python available: 2.7.18
NOTE: preferred version 2.7.9 of lib32-python not available (for item lib32-python-zlib)
NOTE: versions of lib32-python available: 2.7.18
NOTE: preferred version 2.7.9 of lib32-python not available (for item lib32-python-datetime)
NOTE: versions of lib32-python available: 2.7.18
NOTE: preferred version 2.7.9 of lib32-python not available (for item lib32-python-threading)
NOTE: versions of lib32-python available: 2.7.18
NOTE: preferred version 2.7.9 of lib32-python not available (for item lib32-python-sqlite3)
NOTE: versions of lib32-python available: 2.7.18
NOTE: preferred version 2.7.9 of lib32-python not available (for item lib32-python-tkinter)
NOTE: versions of lib32-python available: 2.7.18
NOTE: preferred version 2.7.9 of lib32-python not available (for item lib32-python-codecs)
NOTE: versions of lib32-python available: 2.7.18
NOTE: preferred version 2.7.9 of lib32-python not available (for item lib32-python-distutils)
NOTE: versions of lib32-python available: 2.7.18
NOTE: preferred version 2.7.9 of lib32-python not available (for item lib32-python-difflib)
NOTE: versions of lib32-python available: 2.7.18
NOTE: preferred version 2.7.9 of lib32-python not available (for item lib32-python-contextlib)
NOTE: versions of lib32-python available: 2.7.18
NOTE: preferred version 2.7.9 of lib32-python not available (for item lib32-python-xml)
NOTE: versions of lib32-python available: 2.7.18
NOTE: preferred version 2.7.9 of lib32-python not available (for item lib32-python-netserver)
NOTE: versions of lib32-python available: 2.7.18
NOTE: preferred version 2.7.9 of lib32-python not available (for item lib32-python-ctypes)
NOTE: versions of lib32-python available: 2.7.18
NOTE: preferred version 2.7.9 of lib32-python not available (for item lib32-python-mmap)
NOTE: versions of lib32-python available: 2.7.18
NOTE: preferred version 2.7.9 of lib32-python not available (for item lib32-python-debugger)
NOTE: versions of lib32-python available: 2.7.18
NOTE: preferred version 2.7.9 of lib32-python not available (for item lib32-python-unittest)
NOTE: versions of lib32-python available: 2.7.18
NOTE: preferred version 2.7.9 of lib32-python not available (for item lib32-python-email)
NOTE: versions of lib32-python available: 2.7.18
NOTE: preferred version 2.7.9 of lib32-python not available (for item lib32-python-pkgutil)
NOTE: versions of lib32-python available: 2.7.18
NOTE: preferred version 2.7.9 of lib32-python not available (for item lib32-python-bsddb)
NOTE: versions of lib32-python available: 2.7.18
NOTE: preferred version 2.7.9 of lib32-python not available (for item lib32-python-sqlite3-tests)
NOTE: versions of lib32-python available: 2.7.18
NOTE: preferred version 2.7.9 of lib32-python not available (for item lib32-python-db)
NOTE: versions of lib32-python available: 2.7.18
NOTE: preferred version 2.7.9 of lib32-python not available (for item lib32-python-doctest)
NOTE: versions of lib32-python available: 2.7.18
NOTE: preferred version 2.7.9 of lib32-python not available (for item lib32-python-curses)
NOTE: versions of lib32-python available: 2.7.18
NOTE: preferred version 2.7.9 of lib32-python not available (for item lib32-python-idle)
NOTE: versions of lib32-python available: 2.7.18
NOTE: preferred version 2.7.9 of lib32-python not available (for item lib32-python-misc)
NOTE: versions of lib32-python available: 2.7.18
NOTE: preferred version 2.7.9 of lib32-python not available (for item lib32-python-hotshot)
NOTE: versions of lib32-python available: 2.7.18
NOTE: preferred version 2.7.9 of lib32-python not available (for item lib32-python-json)
NOTE: versions of lib32-python available: 2.7.18
NOTE: preferred version 2.7.9 of lib32-python not available (for item lib32-python-profile)
NOTE: versions of lib32-python available: 2.7.18
NOTE: preferred version 2.7.9 of lib32-python not available (for item lib32-python-pydoc)
NOTE: versions of lib32-python available: 2.7.18
NOTE: preferred version 2.7.9 of lib32-python not available (for item lib32-python-mailbox)
NOTE: versions of lib32-python available: 2.7.18
NOTE: preferred version 2.7.9 of lib32-python not available (for item lib32-python-elementtree)
NOTE: versions of lib32-python available: 2.7.18
NOTE: preferred version 2.7.9 of lib32-python not available (for item lib32-python-gdbm)
NOTE: versions of lib32-python available: 2.7.18
NOTE: preferred version 2.7.9 of lib32-python not available (for item lib32-python-resource)
NOTE: versions of lib32-python available: 2.7.18
NOTE: preferred version 2.7.9 of lib32-python not available (for item lib32-python-compiler)
NOTE: versions of lib32-python available: 2.7.18
NOTE: preferred version 2.7.9 of lib32-python not available (for item lib32-python-xmlrpc)
NOTE: versions of lib32-python available: 2.7.18
NOTE: preferred version 2.7.9 of lib32-python not available (for item lib32-python-html)
NOTE: versions of lib32-python available: 2.7.18
NOTE: preferred version 2.7.9 of lib32-python not available (for item lib32-python-2to3)
NOTE: versions of lib32-python available: 2.7.18
NOTE: preferred version 2.7.9 of lib32-python not available (for item lib32-python-syslog)
NOTE: versions of lib32-python available: 2.7.18
NOTE: preferred version 2.7.9 of lib32-python not available (for item lib32-python-compile)
NOTE: versions of lib32-python available: 2.7.18
NOTE: preferred version 2.7.9 of lib32-python not available (for item lib32-python-tests)
NOTE: versions of lib32-python available: 2.7.18
NOTE: preferred version 2.7.9 of lib32-python not available (for item lib32-python-unixadmin)
NOTE: versions of lib32-python available: 2.7.18
NOTE: preferred version 2.7.9 of lib32-python not available (for item lib32-python-smtpd)
NOTE: versions of lib32-python available: 2.7.18
NOTE: preferred version 2.7.9 of lib32-python not available (for item lib32-python-terminal)
NOTE: versions of lib32-python available: 2.7.18
NOTE: preferred version 2.7.9 of lib32-python not available (for item lib32-python-readline)
NOTE: versions of lib32-python available: 2.7.18
NOTE: preferred version 2.7.9 of lib32-python not available (for item lib32-python-importlib)
NOTE: versions of lib32-python available: 2.7.18
NOTE: preferred version 2.7.9 of lib32-python not available (for item lib32-python-argparse)
NOTE: versions of lib32-python available: 2.7.18
NOTE: preferred version 2.7.9 of lib32-python not available (for item lib32-python-robotparser)
NOTE: versions of lib32-python available: 2.7.18
NOTE: preferred version 2.7.9 of lib32-python not available (for item lib32-python-multiprocessing)
NOTE: versions of lib32-python available: 2.7.18
NOTE: preferred version 2.7.9 of lib32-python not available (for item lib32-python-numbers)
NOTE: versions of lib32-python available: 2.7.18

Build Configuration:
BB_VERSION = "1.28.0"
BUILD_SYS = "x86_64-linux"
NATIVELSBSTRING = "Ubuntu-16.04"
TARGET_SYS = "powerpc64-fsl-linux"
MACHINE = "t1040d4rdb-64b"
DISTRO = "fsl-qoriq"
DISTRO_VERSION = "2.0"
TUNE_FEATURES = "m64 fpu-hard e5500"
TARGET_FPU = "hard"
meta
meta-yocto
meta-yocto-bsp = "HEAD:9a211a4a2c1bfcb292dc97d8dcac149bca9e3f1b"
meta-oe
meta-multimedia
meta-gnome
meta-networking
meta-perl
meta-python
meta-ruby
meta-filesystems
meta-webserver
meta-xfce = "HEAD:dc5634968b270dde250690609f0015f881db81f2"
meta-freescale = "HEAD:7facbdb726e2dda0515e084c2066a4b8dd99c6d2"
meta-freescale-internal = "HEAD:4829293f807e35a1111e79763294fc8b98b97810"
meta-freescale-extra = "HEAD:bee911b027e0480b034674d0ddee3fcb06d2e985"
meta-virtualization = "HEAD:042425c1d98bdd7e44a62789bd03b375045266f5"
meta-java = "HEAD:8b776ac68f9af4596be3824152bcf0bc6b67fa1d"
meta-openstack
meta-openstack-aio-deploy
meta-openstack-compute-deploy
meta-openstack-compute-test-config
meta-openstack-controller-deploy
meta-openstack-controller-test-config
meta-openstack-qemu
meta-openstack-swift-deploy
meta-cloud-services = "HEAD:d8bc0d92d0f741e2ea1e6d3d9bc6b7a091d03cfb"
meta-security = "HEAD:f9367e71f923fc7d2fb600208e2b97535ea41777"
meta-nxp-npi-1701 = "jethro-sdk-v2.0-ga-1701:11975eebce9096a3567d00ba2067a2dbd2ed4d5c"

NOTE: Preparing RunQueue
WARNING: /home/suchita/GCR/v2/QorIQ-SDK-V2.0-20160527-yocto/sources/meta-freescale/recipes-kernel/linux/linux-qoriq_4.1.bb.do_compile is tainted from a forced run
NOTE: Checking sstate mirror object availability (for 60 objects)
NOTE: Executing SetScene Tasks
NOTE: Executing RunQueue Tasks
ERROR: Unable to install packages. Command '/home/suchita/GCR/v2/QorIQ-SDK-V2.0-20160527-yocto/build_t1040d4rdb-64b/tmp/sysroots/x86_64-linux/usr/bin/smart --log-level=warning --data-dir=/home/suchita/GCR/v2/QorIQ-SDK-V2.0-20160527-yocto/build_t1040d4rdb-64b/tmp/work/t1040d4rdb_64b-fsl-linux/fsl-image-core/1.0-r0/rootfs/var/lib/smart install -y lsb@ppc64e5500 net-snmp@ppc64e5500 packagegroup-fsl-mfgtools@all python-core-2.7.18-r1@ppc64e5500 openssh@ppc64e5500 packagegroup-core-ssh-openssh@all tcl@ppc64e5500 udev-extraconf@ppc64e5500 packagegroup-core-boot@t1040d4rdb_64b packagegroup-fsl-benchmark-core@all sqlite3@ppc64e5500 run-postinsts@all udev-rules-qoriq@ppc64e5500 packagegroup-fsl-networking-core@all packagegroup-fsl-tools-core@all libpam@ppc64e5500' returned 1:
Loading cache...
Updating cache... ######################################## [100%]

Computing transaction...error: Can't install libhugetlbfs-1:2.19-r0@ppc64e5500: no package provides python-subprocess


ERROR: Function failed: do_rootfs
ERROR: Logfile of failure stored in: /home/suchita/GCR/v2/QorIQ-SDK-V2.0-20160527-yocto/build_t1040d4rdb-64b/tmp/work/t1040d4rdb_64b-fsl-linux/fsl-image-core/1.0-r0/temp/log.do_rootfs.27036
ERROR: Task 7 (/home/suchita/GCR/v2/QorIQ-SDK-V2.0-20160527-yocto/sources/meta-freescale/recipes-fsl/images/fsl-image-core.bb, do_rootfs) failed with exit code '1'
NOTE: Tasks Summary: Attempted 3349 tasks of which 3178 didn't need to be rerun and 1 failed.
No currently running tasks (3349 of 3350)

Summary: 1 task failed:
/home/suchita/GCR/v2/QorIQ-SDK-V2.0-20160527-yocto/sources/meta-freescale/recipes-fsl/images/fsl-image-core.bb, do_rootfs
Summary: There were 2 WARNING messages shown.
Summary: There were 2 ERROR messages shown, returning a non-zero exit code.

0 件の賞賛
返信