How do I use standalone toolchain to build uboot without yocto?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How do I use standalone toolchain to build uboot without yocto?

1,261 Views
muaxi8
Contributor V

《QorIQ SDK 2.0 Documentation For QorIQ Processors》

3.3.13  There is a toolchain compile for the kernel,I wonder if there is a toolchain compile method for the uboot instead of a Yocto compiler ?

muaxi8_0-1648024269911.png

 

0 Kudos
Reply
1 Reply

1,256 Views
jimmychan
NXP TechSupport
NXP TechSupport

The standalone toolchain to build u-boot is basically same as the method of standalone building kernel. Steps 1-3 are same. Then go to u-boot source dir, then "make" the source code.

0 Kudos
Reply