How can I access the T2080QDS Reference Manual

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How can I access the T2080QDS Reference Manual

1,603件の閲覧回数
antoniogarcia
Contributor I

Where can I find the Reference Manual for the T2080QDS?  Searching for T2080QDS Reference Manual turns up nothing...  I am trying to set the hardware up in a remove lab, and need to understand how to make it power on without requiring someone to physically press the 'Power' switch.  I placed a jumper on the block labeled ATX-Power, and while that did in fact force the ATX power on, it does not cause the board itself to boot.

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,228件の閲覧回数
ufedor
NXP Employee
NXP Employee

Please create a Technical Case:

https://community.freescale.com/thread/381898

0 件の賞賛
返信