what is the power consumption of T2080 in sungle core mode?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

what is the power consumption of T2080 in sungle core mode?

872 Views
ilanwittenberg
Contributor I

what is the power consumption of T2080 in sungle core mode?

Labels (1)
Tags (1)
0 Kudos
1 Reply

485 Views
ufedor
NXP Employee
NXP Employee

Example for one core of the T2080 running at 1533/600/1867MHz with Altivec  power-gated off:

1) from the Table 6. T2080 power dissipation with Altivec power-gated off we have the VDD +SVDD  power consumption at 105C is 17.2W

2) savings for one core (PH10, PH15, PH20) are provided in the Table 10. T2080 Rev 1.1 single core/single cluster low-power mode power savings, 1.0 V 105C

3) overall (three cores powered off):

17.2 - (PH10 + PH15 + PH20) * 3 = 17.2 - (0.82 + 0.23 + 0.35) *3 = 17.2 - 4.2 = 13W

0 Kudos