Getting Error while porting source code to powerpc platform : fatal error: tbb/mutex.h: No such file or directory

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Getting Error while porting source code to powerpc platform : fatal error: tbb/mutex.h: No such file or directory

跳至解决方案
4,273 次查看
vigneshr
Contributor III

Hi All,

I'm porting source code to PowerPC platform, While porting the source code Im facing error like below


#############################################################################################################
In file included from build/debug/vnsw/agent/cfg/cfg_constants.cpp:8:0:

| controller/src/base/trace.h:8:23: fatal error: tbb/mutex.h: No such file or directory

|  #include <tbb/mutex.h>

|                        ^

| compilation terminated.

| scons: *** [build/debug/vnsw/agent/cfg/cfg_constants.o] Error 1

| scons: building terminated because of errors.

| WARNING: exit code 2 from a shell command.

#############################################################################################################

I have included the tbb in the DEPENDS section of bb file, even though tbb is compiled and installed, It is giving the above error. Can anyone let me the know the solution if you aware on this ?? ..

Thanks in advance..

Regards,
Vignesh.

标签 (1)
标记 (3)
0 项奖励
回复
1 解答
3,734 次查看
bpe
NXP Employee
NXP Employee

Bitbake can automatically build a package your software depends on, but it can't

automatically adjust references to it from your code. Check your makefiles to ensure

the headers your software requires are in the compiler search path. Details can

be found here:

Search Path - The C Preprocessor


Have a great day,
Platon

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
2 回复数
3,735 次查看
bpe
NXP Employee
NXP Employee

Bitbake can automatically build a package your software depends on, but it can't

automatically adjust references to it from your code. Check your makefiles to ensure

the headers your software requires are in the compiler search path. Details can

be found here:

Search Path - The C Preprocessor


Have a great day,
Platon

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
3,734 次查看
vigneshr
Contributor III

Thanks bpe.. I resolved the issue.

0 项奖励
回复