PAMU is an analog of MMU, but for peripherals which can act as transaction initiators on the internal bus.
It isolates one bus master from another, restricting their memory access to areas defined by software.
PAMU is necessary for virtualization, if there is a requirement that virtual machines: (a) Utilise DMA-enabled
peripherals; (b) have to run in isolated and controlled memory areas.
Even if you are going to use a single core, but wish to run several virtual machines, which can share
the core, but need to be isolated from one another in memory, PAMU may still be necessary.
If your application does not require virtualization, you can leave PAMU intact.
Refer to T2080RM, Chapter 11 for more information.
Have a great day,
Platon
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------