Error in merging files and directories in NXP Yocto SDK2.0

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Error in merging files and directories in NXP Yocto SDK2.0

Jump to solution
1,821 Views
sandeepk1980
Contributor I

Hi

i have put few directories and files in  files/merge folder by copying

/home/ngntemp/brtr/QorIQ-SDK-V2.0-20160527-yocto/sources/meta-freescale/recipes-extended/merge-files/merge-files/merge/bin

/merge/etc

/merge/usr

 

when i run the   bitbake fsl-image-core,     i am getting this error

Build Configuration:
BB_VERSION = "1.28.0"
BUILD_SYS = "i686-linux"
NATIVELSBSTRING = "Ubuntu-14.04"
TARGET_SYS = "powerpc64-fsl-linux"
MACHINE = "t1040d4rdb-64b"
DISTRO = "fsl-qoriq"
DISTRO_VERSION = "2.0"
TUNE_FEATURES = "m64 fpu-hard e5500"
TARGET_FPU = "hard"
meta
meta-yocto
meta-yocto-bsp = "HEAD:9a211a4a2c1bfcb292dc97d8dcac149bca9e3f1b"
meta-cgl-common = "HEAD:a8a7d8112ac8eb02c5752780dad001ce322291b2"
meta-oe
meta-multimedia
meta-gnome
meta-networking
meta-perl
meta-python
meta-ruby
meta-filesystems
meta-webserver
meta-xfce = "HEAD:dc5634968b270dde250690609f0015f881db81f2"
meta-freescale = "HEAD:7facbdb726e2dda0515e084c2066a4b8dd99c6d2"
meta-freescale-internal = "HEAD:4829293f807e35a1111e79763294fc8b98b97810"
meta-freescale-extra = "HEAD:bee911b027e0480b034674d0ddee3fcb06d2e985"
meta-virtualization = "HEAD:042425c1d98bdd7e44a62789bd03b375045266f5"
meta-java = "HEAD:8b776ac68f9af4596be3824152bcf0bc6b67fa1d"
meta-openstack
meta-openstack-aio-deploy
meta-openstack-compute-deploy
meta-openstack-compute-test-config
meta-openstack-controller-deploy
meta-openstack-controller-test-config
meta-openstack-qemu
meta-openstack-swift-deploy
meta-cloud-services = "HEAD:d8bc0d92d0f741e2ea1e6d3d9bc6b7a091d03cfb"
meta-security = "HEAD:f9367e71f923fc7d2fb600208e2b97535ea41777"

NOTE: Preparing RunQueue
NOTE: Checking sstate mirror object availability (for 7 objects)
NOTE: Executing SetScene Tasks
NOTE: Executing RunQueue Tasks
ERROR: Unable to install packages. Command '/home/ngntemp/brtr/QorIQ-SDK-V2.0-20160527-yocto/build_t1040d4rdb-64b/tmp/sysroots/i686-linux/usr/bin/smart --log-level=warning --data-dir=/home/ngntemp/brtr/QorIQ-SDK-V2.0-20160527-yocto/build_t1040d4rdb-64b/tmp/work/t1040d4rdb_64b-fsl-linux/fsl-image-core/1.0-r0/rootfs/var/lib/smart install -y lsb@ppc64e5500 net-snmp@ppc64e5500 packagegroup-fsl-mfgtools@all python-core-2.7.18-r1@ppc64e5500 openssh@ppc64e5500 packagegroup-core-ssh-openssh@all packagegroup-core-boot@t1040d4rdb_64b monit@ppc64e5500 tcl@ppc64e5500 udev-extraconf@ppc64e5500 merge-files@all packagegroup-fsl-benchmark-core@all sqlite3@ppc64e5500 run-postinsts@all udev-rules-qoriq@ppc64e5500 packagegroup-fsl-networking-core@all packagegroup-fsl-tools-core@all libpam@ppc64e5500' returned 1:
Loading cache...
Updating cache... ######################################## [100%]

Computing transaction...error: Can't install merge-files-1.0-r0@all: no package provides libzebra.so.1()(64bit)


ERROR: Function failed: do_rootfs
ERROR: Logfile of failure stored in: /home/ngntemp/brtr/QorIQ-SDK-V2.0-20160527-yocto/build_t1040d4rdb-64b/tmp/work/t1040d4rdb_64b-fsl-linux/fsl-image-core/1.0-r0/temp/log.do_rootfs.5361
ERROR: Task 7 (/home/ngntemp/brtr/QorIQ-SDK-V2.0-20160527-yocto/sources/meta-freescale/recipes-fsl/images/fsl-image-core.bb, do_rootfs) failed with exit code '1'
NOTE: Tasks Summary: Attempted 3348 tasks of which 3335 didn't need to be rerun and 1 failed.
No currently running tasks (3348 of 3349)

Summary: 1 task failed:
/home/ngntemp/brtr/QorIQ-SDK-V2.0-20160527-yocto/sources/meta-freescale/recipes-fsl/images/fsl-image-core.bb, do_rootfs
Summary: There was 1 WARNING message shown.
Summary: There were 2 ERROR messages shown, returning a non-zero exit code.

 

 

Please provide the solution. one of binary which i am trying to merge in rfs is /usr/bin/zebra. Has it got anything to do with it?

 

 

 

 

 

 

 

 

 

Labels (1)
0 Kudos
Reply
1 Solution
1,817 Views
yipingwang
NXP TechSupport
NXP TechSupport

libzebra.so.1 is provided in package "quagga", please add "quagga" to "IMAGE_INSTALL_append" in sources/meta-freescale/recipes-fsl/images/fsl-image-core.bb, then run the following commands.

$ bitbake fsl-image-core

View solution in original post

0 Kudos
Reply
1 Reply
1,818 Views
yipingwang
NXP TechSupport
NXP TechSupport

libzebra.so.1 is provided in package "quagga", please add "quagga" to "IMAGE_INSTALL_append" in sources/meta-freescale/recipes-fsl/images/fsl-image-core.bb, then run the following commands.

$ bitbake fsl-image-core

0 Kudos
Reply