Enable Linux toolchain in Codewarrior 10.5.1

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Enable Linux toolchain in Codewarrior 10.5.1

3,025 Views
nuj
Contributor I

Hello NXP team,

I am using windows based “CodeWarrior development studio 10.5.1” for developing Linux based project for T1040.

Following this link I  installed Linux GNU Build Tools Service Packs.

 https://community.nxp.com/t5/CodeWarrior-Development-Tools/how-to-develop-an-application-for-T1024/t...

,From

 Help>Install New Software->Work with:(drop list)->FSL PA Build Tools http://freescale.com/lgfiles/updates/Eclipse/PA10_5_1/com.freescale.pa.buildtools_win->; PA GCC LinuxGNU Build Tools Service Packs.

After installation, I restarted codeWarrior , and try to create Linux app project  from ( File -> New -> Codewarrior Linux Project wizard  ) l the Tool chain is still disabled.

When I   look   C:\Freescale\CW_PA_v10.5.1\Cross_Tools there is a new toolchain  folder  “powerpc-linux”.

Now what settings  are further required to enable toolchain and make linux based project ?

Please suggest.

Labels (1)
Tags (1)
0 Kudos
Reply
1 Reply

2,990 Views
nuj
Contributor I

still waiting for reply

 

0 Kudos
Reply