how to develop an application for T1024

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

how to develop an application for T1024

3,108 Views
leventkarakaya
Contributor I

Hello

 

We have bought T1024RDB and CodeWarrior Tap. And I installed CodeWarrior Studio 10.5.1. CodeWarrior contains only Bareboard toolchains. I installed Linux packages from update site. But, I still can not create Linux Project from New Project wizard. At the Build Settings window the Toolchain "Linux: GCC LINUX e5500" is not selectable.

Do you have any documentation or guide about starting development?

I also could not see any document how to boot linux on T1024RDB and how to start development in the package we received.

 

Best Regards

Labels (1)
0 Kudos
Reply
2 Replies

1,944 Views
lana0
Contributor I
0 Kudos
Reply

2,951 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello Levent Karakaya,

First you need to install Linux GNU Build Tools Service Packs, please install it from Help->Install New Software->Work with:(drop list)->FSL PA Build Tools - http://freescale.com/lgfiles/updates/Eclipse/PA10_5_1/com.freescale.pa.buildtools_win->; PA GCC LinuxGNU Build Tools Service Packs.

After installation, please create a Linux app project from File->New->Create a CodeWarrior Linux Project, all QorIQ related platforms use the same toolchain for Linux App project.

After build the Linux APP, you could copy the binary to the target board to execute it directly.

Please refer to SDK document Submit Form  for how to deploy images on the target board.


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply