Does the T1024 have the Aurora interface?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Does the T1024 have the Aurora interface?

ソリューションへジャンプ
1,292件の閲覧回数
Larry5335
Contributor IV

The block diagrams, Ref Man and data sheet all show it. Does Aurora really exist on the T1 series parts?

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
1,133件の閲覧回数
r8070z
NXP Employee
NXP Employee

Have a great day,

The T1024 has the Aurora interface as it is shown in the manual. The Aurora port on the T1024QDS is implemented using the T1024 Aurora interface.

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,134件の閲覧回数
r8070z
NXP Employee
NXP Employee

Have a great day,

The T1024 has the Aurora interface as it is shown in the manual. The Aurora port on the T1024QDS is implemented using the T1024 Aurora interface.

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信