Does the T1024 have the Aurora interface?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Does the T1024 have the Aurora interface?

跳至解决方案
1,228 次查看
Larry5335
Contributor IV

The block diagrams, Ref Man and data sheet all show it. Does Aurora really exist on the T1 series parts?

标签 (1)
标记 (1)
0 项奖励
回复
1 解答
1,069 次查看
r8070z
NXP Employee
NXP Employee

Have a great day,

The T1024 has the Aurora interface as it is shown in the manual. The Aurora port on the T1024QDS is implemented using the T1024 Aurora interface.

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,070 次查看
r8070z
NXP Employee
NXP Employee

Have a great day,

The T1024 has the Aurora interface as it is shown in the manual. The Aurora port on the T1024QDS is implemented using the T1024 Aurora interface.

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复