Developing User/Kernel Space applications for T1024 using Yocto build environment

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Developing User/Kernel Space applications for T1024 using Yocto build environment

1,153 次查看
veerendranathj
Contributor III

How to Develop User/Kernel Space applications for T1024 to access physical memory directly?

Thanks and Regards,

Veerendranath

标签 (1)
标记 (3)
0 项奖励
回复
1 回复

1,062 次查看
Pavel
NXP Employee
NXP Employee

We recommend using CodeWarrior for User/Kernel debugging. CodeWarrior supports viewing for virtual and physical memory addressing.

See the Section 7.7 of the Targeting_PA_Processors.pdf file. This file is available in the CodeWarrior folder.

Have a great day,
Pavel

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复