Developing User/Kernel Space applications for T1024 using Yocto build environment

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Developing User/Kernel Space applications for T1024 using Yocto build environment

1,616件の閲覧回数
veerendranathj
Contributor III

How to Develop User/Kernel Space applications for T1024 to access physical memory directly?

Thanks and Regards,

Veerendranath

ラベル(1)
タグ(3)
0 件の賞賛
返信
1 返信

1,525件の閲覧回数
Pavel
NXP Employee
NXP Employee

We recommend using CodeWarrior for User/Kernel debugging. CodeWarrior supports viewing for virtual and physical memory addressing.

See the Section 7.7 of the Targeting_PA_Processors.pdf file. This file is available in the CodeWarrior folder.

Have a great day,
Pavel

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信