Developing User/Kernel Space applications for T1024 using Yocto build environment

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Developing User/Kernel Space applications for T1024 using Yocto build environment

1,150 Views
veerendranathj
Contributor III

How to Develop User/Kernel Space applications for T1024 to access physical memory directly?

Thanks and Regards,

Veerendranath

Labels (1)
0 Kudos
Reply
1 Reply

1,059 Views
Pavel
NXP Employee
NXP Employee

We recommend using CodeWarrior for User/Kernel debugging. CodeWarrior supports viewing for virtual and physical memory addressing.

See the Section 7.7 of the Targeting_PA_Processors.pdf file. This file is available in the CodeWarrior folder.

Have a great day,
Pavel

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply