Debugging u-boot from DDR T2081 processor

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Debugging u-boot from DDR T2081 processor

Jump to solution
3,872 Views
Ashok0999
Contributor I

Hi Nxp Team,

We have successfully built U-Boot for the NOR flash on the T2081 processor and have reached the U-Boot prompt. However, our Ethernet is currently not operational, making it challenging to perform further debugging.

To facilitate our debugging process, we would like to compile U-Boot to run from DDR, as we can load files into DDR via USB.

Could you please advise on the appropriate compilation options to enable this configuration?

Labels (1)
0 Kudos
Reply
1 Solution
3,807 Views
Oswalag
NXP TechSupport
NXP TechSupport

Hello,

The available procedure is  "RAMboot process using CodeWarrior"

Please check chapter 6 U-Boot RAMboot in T1040D4RDB (It can also be used on boards that do not support SD/eMMC) in the attached guide.

Regards.

View solution in original post

0 Kudos
Reply
2 Replies
3,859 Views
Ashok0999
Contributor I

We require this change because burning U-Boot into NOR via CodeWarrior is taking a significant amount of time. Loading U-Boot into DDR would provide us with a faster turnaround time for our development process.

0 Kudos
Reply
3,808 Views
Oswalag
NXP TechSupport
NXP TechSupport

Hello,

The available procedure is  "RAMboot process using CodeWarrior"

Please check chapter 6 U-Boot RAMboot in T1040D4RDB (It can also be used on boards that do not support SD/eMMC) in the attached guide.

Regards.

0 Kudos
Reply