Core Time Base Clock Configuration (T2080, RCPM)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Core Time Base Clock Configuration (T2080, RCPM)

2,944件の閲覧回数
bernhardsputh
Contributor I

To whom it may concern,

I'm currently in the process of porting our RTOS to the T2080, to be precise the T2080RDB. While implementing the driver for the periodic ticker, for which I use the e6500-core's decrementer circuit (as every core will have it's own ticker), I stumbled across determining of the time base clock, the documentation [1] appears to be unclear with respect to what is happening inside the RCPM:

- Page 2315: RCPM_PCTBCKSELR selects the clock source for each core's time base. Which can either be the RTC clock or the Platform Clock divided by 16.

- Page 2316: RCPM_TBCLKDIVR provides the clock divider for the core time base. Which offers the divisions of 8, 16, 24,  or 32.

Unfortunately, the documentation does not show a diagram that shows the clock distribution / processing path inside the RCPM. Thus my question is whether the RCPM_TBCLKDIVR is always part of the equation? Thus if I select the Platform Clock /16 as time base clock, then this clock will at least be divided again by a factor of 8 by the RCPM_TBCLKDIVR, and thus the resulting time base clock I can get for the timer is Platform Clock / 128.

Best Regards

Bernhard Sputh

[1] QorIQ T2080 Reference Manual, Rev. 2, 02/2016

ラベル(1)
タグ(2)
0 件の賞賛
返信
2 返答(返信)

2,448件の閲覧回数
ufedor
NXP Employee
NXP Employee

The PCTBCKSELRL register have fields that will rout either the platform clock/16 or another clock signal called RTC (that can be supplied from GPIO1[14] pin of the chip) to the Core Timebase. Once the selection is done then we can decide if it is required to further divide the clock frequency by configuring TBCLKDIVR register.

You wrote:

> if I select the Platform Clock /16 as time base clock, then this clock will at least be divided again by a factor of 8 by

> the RCPM_TBCLKDIVR, and thus the resulting time base clock I can get for the timer is Platform Clock / 128.

Correct

0 件の賞賛
返信

2,448件の閲覧回数
parth_gulati
Contributor I

Hi,

How can I configure TBCLKDIVR as it is a read register.

I want to give my time base core as Platform clock/8 is it possible. 

0 件の賞賛
返信