Component DDR4 Schematic?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Component DDR4 Schematic?

Jump to solution
3,325 Views
trevorfox
Contributor III

Hi

I'm having trouble getting this T1042 custom board to work. It uses component DDR4 (instead of DIMM which Dev Board uses) and I want some type of known functional hookup to compare it to.

As I said, the T1042D4RDBDev Board uses DIMM so I can't easily use that one and DIMMs have different functionality than component.

0 Kudos
Reply
1 Solution
3,290 Views
yipingwang
NXP TechSupport
NXP TechSupport

Attached a page with the LS1043A processor and 32-bit DDR4 interface. 64-bit interface uses the same idea and upper-numerated signals.

View solution in original post

2 Replies
3,291 Views
yipingwang
NXP TechSupport
NXP TechSupport

Attached a page with the LS1043A processor and 32-bit DDR4 interface. 64-bit interface uses the same idea and upper-numerated signals.

3,265 Views
trevorfox
Contributor III

Thank you very much!

0 Kudos
Reply