Component DDR4 Schematic?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Component DDR4 Schematic?

ソリューションへジャンプ
3,320件の閲覧回数
trevorfox
Contributor III

Hi

I'm having trouble getting this T1042 custom board to work. It uses component DDR4 (instead of DIMM which Dev Board uses) and I want some type of known functional hookup to compare it to.

As I said, the T1042D4RDBDev Board uses DIMM so I can't easily use that one and DIMMs have different functionality than component.

0 件の賞賛
返信
1 解決策
3,285件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Attached a page with the LS1043A processor and 32-bit DDR4 interface. 64-bit interface uses the same idea and upper-numerated signals.

元の投稿で解決策を見る

2 返答(返信)
3,286件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Attached a page with the LS1043A processor and 32-bit DDR4 interface. 64-bit interface uses the same idea and upper-numerated signals.

3,260件の閲覧回数
trevorfox
Contributor III

Thank you very much!

0 件の賞賛
返信