Communication with FPGA using T1013 IFC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Communication with FPGA using T1013 IFC

Jump to solution
785 Views
ricardofranca
Contributor III

Hello,

I am assessing a possible use of the T1013 in an application that performs access to an FPGA. My hardware/firmware friends use the EBI in 5xxx devices and the eLBC in the P1013; I would like to know if the equivalent in the T1013 would be the IFC.

As the T1023/24/13/14 states "The IFC supports both NAND and NOR flash, as well as a
general purpose memory-mapped interface for connecting low speed ASICs and FPGAs", I was wondering if "low speed" in this context means something similar to the 66MHz of a MPC5777C EBI or something much slower.

Thanks!

Ricardo

0 Kudos
Reply
1 Solution
754 Views
yipingwang
NXP TechSupport
NXP TechSupport

The equivalent in the T1013 is IFC.

"Low speed" in this context means something similar to the 66MHz of a MPC5777C EBI.

 

View solution in original post

1 Reply
755 Views
yipingwang
NXP TechSupport
NXP TechSupport

The equivalent in the T1013 is IFC.

"Low speed" in this context means something similar to the 66MHz of a MPC5777C EBI.