Communication with FPGA using T1013 IFC

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Communication with FPGA using T1013 IFC

跳至解决方案
922 次查看
ricardofranca
Contributor III

Hello,

I am assessing a possible use of the T1013 in an application that performs access to an FPGA. My hardware/firmware friends use the EBI in 5xxx devices and the eLBC in the P1013; I would like to know if the equivalent in the T1013 would be the IFC.

As the T1023/24/13/14 states "The IFC supports both NAND and NOR flash, as well as a
general purpose memory-mapped interface for connecting low speed ASICs and FPGAs", I was wondering if "low speed" in this context means something similar to the 66MHz of a MPC5777C EBI or something much slower.

Thanks!

Ricardo

0 项奖励
回复
1 解答
891 次查看
yipingwang
NXP TechSupport
NXP TechSupport

The equivalent in the T1013 is IFC.

"Low speed" in this context means something similar to the 66MHz of a MPC5777C EBI.

 

在原帖中查看解决方案

1 回复
892 次查看
yipingwang
NXP TechSupport
NXP TechSupport

The equivalent in the T1013 is IFC.

"Low speed" in this context means something similar to the 66MHz of a MPC5777C EBI.