Codewarrior Tap: Failed to reset target, Core not responding.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Codewarrior Tap: Failed to reset target, Core not responding.

5,242 Views
Amit-Kumar
Contributor II

Hi Members,

We have a custom hardware based on T1023RDB, and intend to flash RCW, U-Boot plus other loads for the first time. For that the board is configured for hardcoded RCW option. Parameter [0:8] CFG_RCW_src=0x9E. But the issue we are getting is this:

Following set of options are used to connect/debug for Bare metal project.

AmitKumar_0-1633345554421.png

The error message is this:

AmitKumar_1-1633345622739.png

Updated CCS session logs attached (JTAG Diags enabled).

Please highlight any issues if any from logs.

Tags (1)
0 Kudos
Reply
3 Replies

5,195 Views
ufedor
NXP Employee
NXP Employee

Please provide the processor connection schematics for inspection as searchable PDF.

0 Kudos
Reply

5,159 Views
Amit-Kumar
Contributor II

Sorry for inconvenience. you can close the discussion. I realized that same thread is being discussed by few folks in our company with NXP guys.

0 Kudos
Reply

5,202 Views
Amit-Kumar
Contributor II

@yipingwang : Have a glance please, Thanks!!.

0 Kudos
Reply