Codewarrior Tap: Failed to reset target, Core not responding.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Codewarrior Tap: Failed to reset target, Core not responding.

5,258 次查看
Amit-Kumar
Contributor II

Hi Members,

We have a custom hardware based on T1023RDB, and intend to flash RCW, U-Boot plus other loads for the first time. For that the board is configured for hardcoded RCW option. Parameter [0:8] CFG_RCW_src=0x9E. But the issue we are getting is this:

Following set of options are used to connect/debug for Bare metal project.

AmitKumar_0-1633345554421.png

The error message is this:

AmitKumar_1-1633345622739.png

Updated CCS session logs attached (JTAG Diags enabled).

Please highlight any issues if any from logs.

标记 (1)
0 项奖励
回复
3 回复数

5,211 次查看
ufedor
NXP Employee
NXP Employee

Please provide the processor connection schematics for inspection as searchable PDF.

0 项奖励
回复

5,175 次查看
Amit-Kumar
Contributor II

Sorry for inconvenience. you can close the discussion. I realized that same thread is being discussed by few folks in our company with NXP guys.

0 项奖励
回复

5,218 次查看
Amit-Kumar
Contributor II

@yipingwang : Have a glance please, Thanks!!.

0 项奖励
回复