Classifier_Demo on the T4240 using SDK1.9

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Classifier_Demo on the T4240 using SDK1.9

1,439 次查看
ramkrishnan
Contributor III

I am running SDK 1.9 on the T4240. I was trying to bring up the classifier_demo but it fails saying /dev/dpa_classifier does not exist. I checked in /dev and neither dpa_stats or dpa_classifier exists. I followed the instructions from the Application Node 4785 (which did not have instructions for the rdb , only the qds but I did find the dts files in the non-staging area). Do I need to do anything different ? I am able to run the hello_reflector.

Secondly if I wanted to modify the dpaa demo code for my own application what would be a good place to start. The XML files seem to satisfy a certain static need but to keep it dynamic I would need to configure the fman mac and FQIDs based on user input.

Thank you,

Ram Krishnan

标签 (1)
标记 (2)
0 项奖励
回复
3 回复数

1,199 次查看
ramkrishnan
Contributor III

Adding CONFIG_FSL_DPA_OFFLOAD=y to defconfig in linuxqoriq enables the modules and I am able run the classifier_demo.

Ram

0 项奖励
回复

1,199 次查看
ramkrishnan
Contributor III

Thank you Pavel,

If the Classifier_Demo is not supported do you know of any sample code to do Table Key based lookups which does not use the /dev/classif driver interface.

Thank you,

Ram Krishnan

0 项奖励
回复

1,199 次查看
Pavel
NXP Employee
NXP Employee

Sorry for delay.

I have checked SDK 1.9 and 2.0. It looks like that these SDK do not support Classifier_Demo on the T4240 board.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复