Can we run GUI based Linux on T4240 processor?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can we run GUI based Linux on T4240 processor?

2,535件の閲覧回数
A-R
Contributor II

Hi,

Is there any support of GUI based linux(Like ubuntu) to run on T4240 processor?

Also I need some document that can guide me how to connect GPU with T4240 processor. 

Also I need to know if there is any power architecture processor of NXP that have GPU to run GUI based Linux(Like ubuntu) on it? 

0 件の賞賛
返信
2 返答(返信)

2,395件の閲覧回数
matevzlangus
Contributor III

Hi,

we are running Gentoo with GUI on T4 for fun. Libreoffice, web browser, VLC... very fast desktop but... fun only

0 件の賞賛
返信

2,526件の閲覧回数
ufedor
NXP Employee
NXP Employee

> Is there any support of GUI based linux(Like ubuntu) to run on T4240 processor?

There is no GUI support for the T4240.

 

> is any power architecture processor of NXP that have GPU

T104x has DIU - Display Interface Unit.