osek part number

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
3,619件の閲覧回数
hotashu
Contributor III

I am intresting in osek. i find this link:</p>


http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=OSEKTURBO&tab=Buy_Parametric_Tab&from...

but there is no description about the part number list.
for example:
CWX-OSK-D100K-DL
CWX-OSK-D10K-DL
CWX-OSK-D1K-DL
CWX-OSK-D200-DL
CWX-OSK-D200K-DL
CWX-OSK-D2MIL-DL
CWX-OSK-D500K-DL
CWX-OSK-UNLTD-DL


the price is different for each of them.
it is very appreciated if anybody can tell me the different.

ラベル(1)
0 件の賞賛
返信
1 解決策
3,349件の閲覧回数
leeexum
NXP Employee
NXP Employee

Hello and thanks for your interest in OSEK.  The license options you list are for distribution (royalty) licensing increments. Pricing for those royalties increases based on production volumes of products using OSEK within the application.  We have asked our Automotive Software team to elaborate further.

Regards,

Lee Exum

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
3,349件の閲覧回数
trytohelp
NXP Employee
NXP Employee

Hi Hotas,

I was in contact with the Product Manager regarding this problem.

We need to know exactly the processor you want to use.

Without this information we could not provide you an answer.

Regards

Pascal

0 件の賞賛
返信
3,350件の閲覧回数
leeexum
NXP Employee
NXP Employee

Hello and thanks for your interest in OSEK.  The license options you list are for distribution (royalty) licensing increments. Pricing for those royalties increases based on production volumes of products using OSEK within the application.  We have asked our Automotive Software team to elaborate further.

Regards,

Lee Exum

0 件の賞賛
返信
3,349件の閲覧回数
hotashu
Contributor III

thank you.

BTW, is our latest osek version  v2.5.1?

0 件の賞賛
返信
3,349件の閲覧回数
trytohelp
NXP Employee
NXP Employee

Hi,

I've checked with a colleague.

To provide correct answer we need to know exactly the architecture/processor used ?

Pascal

0 件の賞賛
返信