need help for floating license

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

need help for floating license

ソリューションへジャンプ
3,818件の閲覧回数
alexx
Contributor I
Hi, i register my product and obtain the license.dat
 
I need to use the floating license
 
server: linux (debian)
client: windows
 
I put license.dat (windows version) in the /flexlm directory on windows client
 
How can i install the license manager in my linux server (debian)??? i get the tar file, extract the files but i can't start the service.... anyone could help me?
 
 
thank you
bye
ラベル(1)
0 件の賞賛
返信
1 解決策
2,056件の閲覧回数
stanish
NXP Employee
NXP Employee
Currently the only supported Linux distribution is Linux RedHat 8. Other distributions are not supported so the licensing manager might not work
(see http://www.freescale.com/webapp/sps/site/overview.jsp?code=CW_LICENSE_FLEXDOWN&fsrch=1)

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,057件の閲覧回数
stanish
NXP Employee
NXP Employee
Currently the only supported Linux distribution is Linux RedHat 8. Other distributions are not supported so the licensing manager might not work
(see http://www.freescale.com/webapp/sps/site/overview.jsp?code=CW_LICENSE_FLEXDOWN&fsrch=1)
0 件の賞賛
返信