need help for floating license

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

need help for floating license

Jump to solution
4,679 Views
alexx
Contributor I
Hi, i register my product and obtain the license.dat
 
I need to use the floating license
 
server: linux (debian)
client: windows
 
I put license.dat (windows version) in the /flexlm directory on windows client
 
How can i install the license manager in my linux server (debian)??? i get the tar file, extract the files but i can't start the service.... anyone could help me?
 
 
thank you
bye
Labels (1)
0 Kudos
Reply
1 Solution
2,917 Views
stanish
NXP Employee
NXP Employee
Currently the only supported Linux distribution is Linux RedHat 8. Other distributions are not supported so the licensing manager might not work
(see http://www.freescale.com/webapp/sps/site/overview.jsp?code=CW_LICENSE_FLEXDOWN&fsrch=1)

View solution in original post

0 Kudos
Reply
1 Reply
2,918 Views
stanish
NXP Employee
NXP Employee
Currently the only supported Linux distribution is Linux RedHat 8. Other distributions are not supported so the licensing manager might not work
(see http://www.freescale.com/webapp/sps/site/overview.jsp?code=CW_LICENSE_FLEXDOWN&fsrch=1)
0 Kudos
Reply