Inquiries about the CodeWarrier license.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Inquiries about the CodeWarrier license.

ソリューションへジャンプ
6,752件の閲覧回数
kwru
Contributor III

I have been issued a license for the CodeWarrier dongle and use it.

Until now, it was possible to copy the license to a new PC and use it as the same dongle USB.

Recently, I copied the license to a new PC and used it as the same dongle USB, so it doesn't work.

I don't know the difference between a PC that has been operable so far and a PC that I recently purchased.

The license has been purchased for more than five years.

Licenses still work well on existing PCs.

I want to move my work environment to a new PC, what should I do?

タグ(2)
0 件の賞賛
返信
1 解決策
6,650件の閲覧回数
jorge_plascencia
NXP TechSupport
NXP TechSupport

Some Windows 10 computers will not allow the Dongle to comunicate with the CodeWarrior Software, pelase genearte the License with the MAC addrress of the computer that you will be using CodeWarrior with.

Dongles will be discontinued latter this year.

元の投稿で解決策を見る

0 件の賞賛
返信
6 返答(返信)
6,670件の閲覧回数
stanish
NXP Employee
NXP Employee

Hello,

Yes, you can migrate the dongle license as you described.

I suspect there is an issue with dongle driver.

I'd recommend you reinstall the drivers:

https://www.nxp.com/webapp/sps/download/license.jsp?colCode=CWX-FLEX-DD-STD

and run LMtools (64bit)

https://www.nxp.com/lgfiles/licensing/LMTOOLS-64BIT.zip

can you see the flexID detected (as depicted on page 5. of document below)?

https://www.nxp.com/docs/en/supporting-information/DongleQS.pdf

 

Hope it helps.

Stan

0 件の賞賛
返信
6,664件の閲覧回数
kwru
Contributor III

I installed LMtools, dongle driver, and flexID.

It was also confirmed that the dongle driver was recognized with the flexID as shown in page 5 of the attached document.

It still doesn't working.

0 件の賞賛
返信
6,658件の閲覧回数
stanish
NXP Employee
NXP Employee

Hi,

could you make sure the valid license.dat (locked to the FlexID printed on USB dongle) is located in "<CodeWarrior for MCU>\MCU\license.dat"

Also please check the license path -  system variable LM_LICENSE_FILE (type "set LM_LICENSE" in windows terminal/command line)

if there a path to an alternative codewarrior version installed on the computer wrong license could be used.

Stan

0 件の賞賛
返信
6,653件の閲覧回数
kwru
Contributor III

The license.dat file is located in the correct location.

(C:\freescale\CW MCU v10.7\MCU\license.dat)

 

There may be a problem with CodeWarrier 2.1 installed on the PC.

So can you explain this part in more detail?
->  Also please check the license path - system variable LM_LICENSE_FILE (type "set LM_LICENSE" in windows terminal/command line)

How can I check the license path?

0 件の賞賛
返信
6,651件の閲覧回数
jorge_plascencia
NXP TechSupport
NXP TechSupport

Some Windows 10 computers will not allow the Dongle to comunicate with the CodeWarrior Software, pelase genearte the License with the MAC addrress of the computer that you will be using CodeWarrior with.

Dongles will be discontinued latter this year.

0 件の賞賛
返信
6,742件の閲覧回数
kwru
Contributor III

I am using CodeWarrior 10.7 version.

0 件の賞賛
返信