Inquiries about the CodeWarrier license.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Inquiries about the CodeWarrier license.

Jump to solution
6,575 Views
kwru
Contributor III

I have been issued a license for the CodeWarrier dongle and use it.

Until now, it was possible to copy the license to a new PC and use it as the same dongle USB.

Recently, I copied the license to a new PC and used it as the same dongle USB, so it doesn't work.

I don't know the difference between a PC that has been operable so far and a PC that I recently purchased.

The license has been purchased for more than five years.

Licenses still work well on existing PCs.

I want to move my work environment to a new PC, what should I do?

Tags (2)
0 Kudos
Reply
1 Solution
6,473 Views
jorge_plascencia
NXP TechSupport
NXP TechSupport

Some Windows 10 computers will not allow the Dongle to comunicate with the CodeWarrior Software, pelase genearte the License with the MAC addrress of the computer that you will be using CodeWarrior with.

Dongles will be discontinued latter this year.

View solution in original post

0 Kudos
Reply
6 Replies
6,493 Views
stanish
NXP Employee
NXP Employee

Hello,

Yes, you can migrate the dongle license as you described.

I suspect there is an issue with dongle driver.

I'd recommend you reinstall the drivers:

https://www.nxp.com/webapp/sps/download/license.jsp?colCode=CWX-FLEX-DD-STD

and run LMtools (64bit)

https://www.nxp.com/lgfiles/licensing/LMTOOLS-64BIT.zip

can you see the flexID detected (as depicted on page 5. of document below)?

https://www.nxp.com/docs/en/supporting-information/DongleQS.pdf

 

Hope it helps.

Stan

0 Kudos
Reply
6,487 Views
kwru
Contributor III

I installed LMtools, dongle driver, and flexID.

It was also confirmed that the dongle driver was recognized with the flexID as shown in page 5 of the attached document.

It still doesn't working.

0 Kudos
Reply
6,481 Views
stanish
NXP Employee
NXP Employee

Hi,

could you make sure the valid license.dat (locked to the FlexID printed on USB dongle) is located in "<CodeWarrior for MCU>\MCU\license.dat"

Also please check the license path -  system variable LM_LICENSE_FILE (type "set LM_LICENSE" in windows terminal/command line)

if there a path to an alternative codewarrior version installed on the computer wrong license could be used.

Stan

0 Kudos
Reply
6,476 Views
kwru
Contributor III

The license.dat file is located in the correct location.

(C:\freescale\CW MCU v10.7\MCU\license.dat)

 

There may be a problem with CodeWarrier 2.1 installed on the PC.

So can you explain this part in more detail?
->  Also please check the license path - system variable LM_LICENSE_FILE (type "set LM_LICENSE" in windows terminal/command line)

How can I check the license path?

0 Kudos
Reply
6,474 Views
jorge_plascencia
NXP TechSupport
NXP TechSupport

Some Windows 10 computers will not allow the Dongle to comunicate with the CodeWarrior Software, pelase genearte the License with the MAC addrress of the computer that you will be using CodeWarrior with.

Dongles will be discontinued latter this year.

0 Kudos
Reply
6,565 Views
kwru
Contributor III

I am using CodeWarrior 10.7 version.

0 Kudos
Reply