I want to configure License server with multiple floating licenses, can I know the steps the involved?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

I want to configure License server with multiple floating licenses, can I know the steps the involved?

1,148 次查看
umeshpiparava
Contributor II

Hi,

 

We have a License server configured with 1 floating License. It is working fine.

I want to configure the License server with multiple floating licenses,

can I know the steps the involved?

While generating License file, should I use same port number or different one?

 

Thanks,

Karthi

标签 (1)
标记 (2)
0 项奖励
回复
1 回复

1,007 次查看
stanish
NXP Employee
NXP Employee

Hello Karthi,

AFAIK the floating license file should be locked to the same locking ID for all the seats (e.g. server MAC or Disc Volume ID)

TCP port and server name/IP address is fully configurable and it's typically common for all the seats and you can change them any time.

Your license.dat on the server side typically contains common SERVER/DAEMON lines and merged features from all the floating license.dat files (locked to same ID)

SERVER tokyo 17007ea8 1700
VENDOR metrowks
USE_SERVER
FEATURE f1 xyzd 1.000 01-jan-99 5 16BE40E1DAEEEDA8798D ""
FEATURE f2..
FEATURE f3..‍‍‍‍‍‍

Hope it helps.

Stan

0 项奖励
回复