I want to configure License server with multiple floating licenses, can I know the steps the involved?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I want to configure License server with multiple floating licenses, can I know the steps the involved?

1,206 Views
umeshpiparava
Contributor II

Hi,

 

We have a License server configured with 1 floating License. It is working fine.

I want to configure the License server with multiple floating licenses,

can I know the steps the involved?

While generating License file, should I use same port number or different one?

 

Thanks,

Karthi

Labels (1)
Tags (2)
0 Kudos
Reply
1 Reply

1,065 Views
stanish
NXP Employee
NXP Employee

Hello Karthi,

AFAIK the floating license file should be locked to the same locking ID for all the seats (e.g. server MAC or Disc Volume ID)

TCP port and server name/IP address is fully configurable and it's typically common for all the seats and you can change them any time.

Your license.dat on the server side typically contains common SERVER/DAEMON lines and merged features from all the floating license.dat files (locked to same ID)

SERVER tokyo 17007ea8 1700
VENDOR metrowks
USE_SERVER
FEATURE f1 xyzd 1.000 01-jan-99 5 16BE40E1DAEEEDA8798D ""
FEATURE f2..
FEATURE f3..‍‍‍‍‍‍

Hope it helps.

Stan

0 Kudos
Reply