How to get a license with codewarrior?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How to get a license with codewarrior?

跳至解决方案
4,386 次查看
johnnywang
Contributor I

I've used  CodeWarrior for Power Architecture V10.5.0 with an evaluation license before two weeks.And now it presentation that: Debugger license error.

I use the codewarrior software only for load P2020 u-boot file to the Flash,but now It seems that I can't use the software.what can I do for it? Is't that it must buy a license for the further using when I load boot file to the P2020's Flash?

0 项奖励
回复
1 解答
4,292 次查看
lisettelozano
NXP Employee
NXP Employee

Hi Johnny, 

If you are using an evaluation license, you should have generated a license.dat file and place it in the installation folder. For the Power Architecture v10.5 normally should be placed in C:\Freescale\CW_PA_v10.5\PA.

You can try to download one here https://www.nxp.com/webapp/swlicensing/sso/downloadSoftware.sp?catid=CWX-ARCHT-EX  or if already exist, you can retrieve this file from there also. Note that this version can be in the Previous tab on the page that will appear after logging in that link. 

Best Regards, 

Paulina

在原帖中查看解决方案

0 项奖励
回复
3 回复数
4,292 次查看
lisettelozano
NXP Employee
NXP Employee

Hello Johnny, 

Checking your account, I do not see any license generated for v10.5; so first it would be good to see which license is the one that you are using. Could you please provide it?

Best Regards, 

Paulina

0 项奖励
回复
4,292 次查看
johnnywang
Contributor I

I'm sorry,I’m using an  evaluation  CW software now,there is no license.And it doesn't work now.

0 项奖励
回复
4,293 次查看
lisettelozano
NXP Employee
NXP Employee

Hi Johnny, 

If you are using an evaluation license, you should have generated a license.dat file and place it in the installation folder. For the Power Architecture v10.5 normally should be placed in C:\Freescale\CW_PA_v10.5\PA.

You can try to download one here https://www.nxp.com/webapp/swlicensing/sso/downloadSoftware.sp?catid=CWX-ARCHT-EX  or if already exist, you can retrieve this file from there also. Note that this version can be in the Previous tab on the page that will appear after logging in that link. 

Best Regards, 

Paulina

0 项奖励
回复