Floating license connection error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Floating license connection error

3,863件の閲覧回数
hansung_jung
Contributor III

I had used an evaluation version of CodeWarrior® Development Studio for HCS12(X), I purchased a license of CWP-STANDARD-FL-ND a few days ago.

I conducted registration and generated a license key of Development Studio for HCS12(X).

And then I set up the license server environment.

(referring to "FLTLICINSTWINBR.pdf", at the client-side, I pasted "license.dat" from the server and set system variable)

Host and client PC are combined through a local network.

However, I got this message, when I try to compile.

error.jpg

At that time, the license server's status is like below.

1.jpg

2.jpg

3.jpg

4.jpg

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

3,765件の閲覧回数
stanish
NXP Employee
NXP Employee

Hi,

For debug this issue, please try to add [email protected] into LM_LICENSE_FILE environment variable.

CodeWarrior will first have a look there for the valid license before it checks the license.dat in the local folder.

Stan

0 件の賞賛
返信

3,788件の閲覧回数
jorge_plascencia
NXP TechSupport
NXP TechSupport

HI Hansung

it seems that the client machine is not connecting to the server, can you share a screen capture of the variable you created and also the location where the license file has been hosted on the client side.

Regards,

0 件の賞賛
返信